Other Parts Discussed in Thread: TMS570LS0332, HALCOGEN
Hi,
I am using TMS570LS0332 in my design. I would like to the reason for the following behavior. I am getting "undefEntry" exception. When i checked the code in disassembly, it looks as follows.
00020000: ???? Memory map prevented reading 0x00020000 [code=0x20000]
00020004: ???? Memory map prevented reading 0x00020004 [code=0x20000]
00020008: ???? Memory map prevented reading 0x00020008 [code=0x20000]
96 linREG->MBRSR = (uint32)8191U;
0002000c: ???? Memory map prevented reading 0x0002000C [code=0x20000]
00020010: ???? Memory map prevented reading 0x00020010 [code=0x20000]
00020014: ???? Memory map prevented reading 0x00020014 [code=0x20000]
00020018: ???? Memory map prevented reading 0x00020018 [code=0x20000]
MPU is disabled in the HALCoGen.
Thanks & Best Regards,
Sreekanth Challa