This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Programming BOOTCFG register: Application not booting up

Hi,

I am using TIVA C 129X Dev board and trying to program BOOTCFG register , to invoke bootloader based on the value of PB4 on power up. After programming the Bootcfg register, i did a full power reset, and the value of BOOTCFG register is showing correctly (read back from CCS).

I loaded the blinky example to board and the LED is blinking. If i press reset or do full power reset, The blinky is not booting up. To check, I tried updating FW using LM flash programmer and its not able to communicate with Board. 

Its working every time when i load it from CCS by pressing the debug option. But when i do a reset its not.. 

What does it mean?

Code is given below:

void progBootCfg_reg()
{



if (( FLASH_BOOTCFG_R & FLASH_BOOTCFG_NW ) != 0 )
{

   // Write the desired boot configuration to the FMD register
   FLASH_FMD_R =0x7FFF30FE ;  // (FLASH_BOOTCFG_PORT_B | FLASH_BOOTCFG_PIN_4 | FLASH_BOOTCFG_POL | FLASH_BOOTCFG_DBG1);

  // Write the address of the register which we wish to commit
  FLASH_FMA_R = 0x75100000;

  // Write to non-volatile register (KEY + COMT bit)
  FLASH_FMC_R = (FLASH_FMC_WRKEY | FLASH_FMC_COMT);//Poll COMT bit in the FMC register until the commit operation is complete

  while((HWREG(FLASH_FMC_R) & FLASH_FMC_COMT))
  {
  }

}

}

Should I configure any other things to get it working?

  • Hello Sajmal,

    I understand that in this case since there is no API, DRMs have to be used, but the HWREG API is easier to understand than the register address defines that are used in you code. Also please use syntax highlighter while pasting code as it makes it easy to browse through the code.

    From the value written to FMD register, PB4 line should be held low during reset to enter ROM Bootloader. Are you holding PB4 low during reset?

    Thanks,
    Sai
  • Thaks sai,

    I connected PB4 directly to Ground and pressed reset button  or did a power cycle . Should I use any resistor to do it?