This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C123 program starts out in the fault ISR



Hello,

I have been trying to build my own project using the TM4C123 launchpad. I have finally been able to get my code to compile but when I run it I am starting in the fault ISR. I placed a breakpoint at the start of main() but it was never hit. So it is faulting before my code even executes.

When I pause my code and look at the NVIC_FAULT_STAT register I find that I am getting a

NVIC_FAULT_START_IERR

Any ideas on what is going on here? This is my code. (although I don't think any of it is ever getting executed)

/*
 * main.c
 */

#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_memmap.h"
#include "driverlib/gpio.h"
#include "driverlib/sysctl.h"
#include "driverlib/pin_map.h"
#include "driverlib/ssi.h"
#include "driverlib/sysctl.h"
#include "driverlib/uart.h"
#include "utils/uartstdio.h"
//#include "LCDDriver/ILI9341_SPI.h"

//*****************************************************************************
//
// Blink the on-board LED.
//
//*****************************************************************************
int
main(void)
{
    volatile uint32_t ui32Loop;

    //uint32_t pui32DataTx[NUM_SSI_DATA];
    //uint32_t pui32DataRx[NUM_SSI_DATA];
    //uint32_t ui32Index;

    //
    // Set the clocking to run directly from the external crystal/oscillator.
    // TODO: The SYSCTL_XTAL_ value must be changed to match the value of the
    // crystal on your board.
    //

    SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | SYSCTL_OSC_MAIN |
                  SYSCTL_XTAL_16MHZ);

    //
    // Set up the serial console to use for displaying messages.  This is
    // just for this example program and is not needed for SSI operation.
    //
    //InitConsole();

    //
    // Display the setup on the console.
    //
    //UARTprintf("SSI ->\n");
    //UARTprintf("  Mode: SPI\n");
    //UARTprintf("  Data: 8-bit\n\n");

    //
    // The SSI0 peripheral must be enabled for use.
    //
    SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI0);

    //
    // For this example SSI0 is used with PortA[5:2].  The actual port and pins
    // used may be different on your part, consult the data sheet for more
    // information.  GPIO port A needs to be enabled so these pins can be used.
    // TODO: change this to whichever GPIO port you are using.
    //
    SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);

    //
    // Configure the pin muxing for SSI0 functions on port A2, A3, A4, and A5.
    // This step is not necessary if your part does not support pin muxing.
    // TODO: change this to select the port/pin you are using.
    //
    GPIOPinConfigure(GPIO_PB7_SSI2TX);
    GPIOPinConfigure(GPIO_PB6_SSI2RX);
    GPIOPinConfigure(GPIO_PB4_SSI2CLK);

    //
    // Configure the GPIO settings for the SSI pins.  This function also gives
    // control of these pins to the SSI hardware.  Consult the data sheet to
    // see which functions are allocated per pin.
    // The pins are assigned as follows:
    //      PA5 - SSI0Tx
    //      PA4 - SSI0Rx
    //      PA3 - SSI0Fss
    //      PA2 - SSI0CLK
    // TODO: change this to select the port/pin you are using.
    //
    GPIOPinTypeSSI(GPIO_PORTB_BASE, GPIO_PIN_7 | GPIO_PIN_6 | GPIO_PIN_4);

    //
    // Configure and enable the SSI port for SPI master mode.  Use SSI0,
    // system clock supply, idle clock level low and active low clock in
    // freescale SPI mode, master mode, 1MHz SSI frequency, and 8-bit data.
    // For SPI mode, you can set the polarity of the SSI clock when the SSI
    // unit is idle.  You can also configure what clock edge you want to
    // capture data on.  Please reference the datasheet for more information on
    // the different SPI modes.
    //
    SSIConfigSetExpClk(SSI2_BASE, SysCtlClockGet(), SSI_FRF_MOTO_MODE_0,
                       SSI_MODE_MASTER, 1000000, 8);

    SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
    SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
    SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOC);
    GPIOPinTypeGPIOOutput(GPIO_PORTB_BASE, GPIO_PIN_3);
    GPIOPinWrite(GPIO_PORTB_BASE, GPIO_PIN_3, GPIO_PIN_3);
    //
    // Enable the SSI0 module.
    //
    SSIEnable(SSI0_BASE);

    //
    // Read any residual data from the SSI port.  This makes sure the receive
    // FIFOs are empty, so we don't read any unwanted junk.  This is done here
    // because the SPI SSI mode is full-duplex, which allows you to send and
    // receive at the same time.  The SSIDataGetNonBlocking function returns
    // "true" when data was returned, and "false" when no data was returned.
    // The "non-blocking" function checks if there is any data in the receive
    // FIFO and does not "hang" if there isn't.
    //
    uint32_t data_value;
    while(SSIDataGetNonBlocking(SSI0_BASE, &data_value))
    {
    }

    //
    // Delay for a bit.
    //
    for(ui32Loop = 0; ui32Loop < 200000; ui32Loop++)
    {
    }


    //ILI9341_begin();
    //setBgColor(COLOR_RED);

    //
    // Enable the GPIO port that is used for the on-board LED.
    //
    /*
    SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);

    //
    // Check if the peripheral access is enabled.
    //
    while(!SysCtlPeripheralReady(SYSCTL_PERIPH_GPIOF))
    {
    }

    //
    // Enable the GPIO pin for the LED (PF3).  Set the direction as output, and
    // enable the GPIO pin for digital function.
    //
    GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, GPIO_PIN_3);

    //
    // Loop forever.
    //
    while(1)
    {
        //
        // Turn on the LED.
        //
        GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_3, GPIO_PIN_3);

        //
        // Delay for a bit.
        //
        for(ui32Loop = 0; ui32Loop < 200000; ui32Loop++)
        {
        }

        //
        // Turn off the LED.
        //
        GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_3, 0x0);

        //
        // Delay for a bit.
        //
        for(ui32Loop = 0; ui32Loop < 200000; ui32Loop++)
        {
        }
    }
    */
}

Thanks,

Jonathan L Clark