Other Parts Discussed in Thread: TM4C123GH6PGE
Hello
Am I right that two capcitors (1 *0.1uf and 1*1 uf ) should be placed on each VDD pin of TM4C123G ?
Considering we run power supply on 3.3V, can you confirm the value that VDD should get ?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TM4C123GH6PGE
Hello
Am I right that two capcitors (1 *0.1uf and 1*1 uf ) should be placed on each VDD pin of TM4C123G ?
Considering we run power supply on 3.3V, can you confirm the value that VDD should get ?
Thanks
Robert,
Your post is probably usefull but I didn't understand and visualize it well.
It would be good to have a simple scheme even made on a piece of paper and taken with a camera to better visualize your prposal to place capacitor on which pin exactly.
Chrischina said:this : " the first capacitor is the ground and power plane"
The ground and power planes form a capacitor (Two metal planes separated by a dielectric). It is a small capacitor since the planes are far apart but it does play a role. Basically I'm suggesting you don't try to save money by using a two layer board or otherwise removing the power planes.
Chrischina said:"0u01 and a 0u1"
That's a standard notation for capacitance values. The SI prefix replaces the decimal notator (u replaces the Greek micron since it is similar in appearance and present on a standard keyboard). It saves confusion due to
Robert