Hi,
I refer to the TRM for TMS57012x - spnu515b.
The description of the field TICKENA in register TICKCNT reads:
When the tick counter is enabled it starts down-counting from its current value. When TICKENA
goes from 0 to 1, the tick counter is automatically loaded with the contents of TICKVALUE.
How can the counter start from its current value if it is reloaded at the same time? Am I missing something?
In case the latter sentence is the correct one, the question arises whether the (re)load on (re)enable is accompanied by a toggle of the trigger signal.
Regards,
Rainald