This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How do erase flash after executing program line NOXTAL and MOSC is silent.

Guru 56218 points

Not sure how a single register command disabled MOSC but LMF could no longer write to flash memory after doing so. 

LMF gives message: **ERROR** Unable to initialize target -0!  

Seemingly PIOS should be the source oscillator for MCU flash write and DAP connection after LMF does an unlock and erases flash memory.  The NOXTAL bit=1 (no crystal present) after POR and datasheet mentions  to clear the bits like below start MCU from default oscillator PIOS.

Even after unlock the EK-TM4C1294i3-XL MOSC will not start as if NOXTAL is still the case but why if LMF has erased flash memory?

Can MCU JTAG erase flash where ICDI seems to be failing to erase flash during unlock procedure?

command that killed the beast:

/* When an attached crystal clear PWRDWN and NOXTAL bits MOSCTL register*/
HWREG(SYSCTL_MOSCCTL) &= ~(SYSCTL_MOSC_PWR_DIS | SYSCTL_MOSC_NO_XTAL);

  • Hello BP101,

    The datasheet description of the NOXTAL bit is:
    "Provides the user control over the power drawn from the main oscillator
    circuit. This bit should be set when either crystal or single-ended mode
    is being used.

    If the application needs MOSC, this bit should be cleared."

    So, shutting down MOSC (or at least the XTAL circuit) is what it is intended to do . Did you enable PIOSC and set it as your system clock prior to shutting it down? If not, then there is no system clock which is why LM Flashprogrammer can't connect. You will have the same issue with JTAG as with ICDI since you no longer have a system clock.
  • Hi Chuck,

    Clearing the NOXTAL bit should not have had effect of killing PIOSC which is set default oscillator in RSCLKCFG for flash and EEROM until MOSC is set as the clock source. Either way there must be some way to erase flash in PIOSC clock mode just after POR.

    I just cleared the bit as it said to do assuming PIOSC was default clock source prior to configuring MOSC as the run source in RSCLKCFG REG 11, 0x0b

    MOSCCTL REG10 0x7c

    NOXTAL[2]: 0  RST=1 This bit should be cleared when a crystal or oscillator is connected to the OSC0 and OSC1 inputs, regardless of whether or not the MOSC is used or powered down.

    This routine was last flash but had the PLLPWR enable bit in the wrong position and PYSDIV was set 4 not 3, both are corrected below. That N+1 is vague since the clock tree shows [4] and clock selection division tables. Perhaps don't show PHYSDIV already at 4 in tables then also state N+1 and show the same N+1 in register programming.  That method is highly confusing where N=3 not N=4 as is shown in the crystal frequency division and selection tables. 

    	 /* Set the MOSC for High frequency oscillator */
    	 HWREG(SYSCTL_MOSCCTL) |= SYSCTL_MOSC_HIGHFREQ;
    	 /* When attached crystal clear PWRDWN and NOXTAL bits MOSCTL register*/
    	 HWREG(SYSCTL_MOSCCTL) &= ~(SYSCTL_MOSC_PWR_DIS | SYSCTL_MOSC_NO_XTAL);
    	 /* Wait until the MOSC indicates fully powered up */
    	 while((!HWREG(SYSCTL_RIS) & SYSCTL_INT_MOSC_PUP))
    	 {
    	 }
    	 /* Source OSCSRC[23:20] POR defaults PIOSC. */
    	 HWREG(SYSCTL_RSCLKCFG) |= SYSCTL_RSCLKCFG_OSCSRC_MOSC;
    
    	 /* When writing to PLLFRE0 Power down PLLPWR[23] */
    	 HWREG(SYSCTL_PLLFREQ0) |= 0x00000000;
    	 /* Set PLL MINT=96, MFRAC=0, PLLPWR=0 enable bits */
    	 HWREG(SYSCTL_PLLFREQ0) |= 0x60;
    	 /* Set PLL reduce jitter Q=0 and N=4  */
    	 HWREG(SYSCTL_PLLFREQ1) |= (0x0 | 0x4);
    	 /* Power up the PLLPWR[23] */
    	 HWREG(SYSCTL_PLLFREQ0) |= 0x00100000;
    
    	 /* Refresh Flash/EEROM speed  FWS/EWS[25:22]&[9:6]=0x5,
    	  * FBCHT/EBCHT[19:16]&[3:0]=0x6 */
    	 HWREG(SYSCTL_MEMTIM0) |= 0x01950195;
    	 /* Check if TReady LOCK status */
         while(HWREG(SYSCTL_PLLSTAT) != 0x1)
         {
         }
    	 /* Write the PSYSDIV PLL divisor N+1 [9:0]=0x3. */
    	 HWREG(SYSCTL_RSCLKCFG) |=  0x3;
    
    	 /* Enable MEMTIMU[31],NEWFREQ[30],USEPLL[28] Q0/Q1 Indicate to use 480Mhz PLL */
    	 HWREG(SYSCTL_RSCLKCFG) |=
    			 (SYSCTL_RSCLKCFG_MEMTIMU | SYSCTL_RSCLKCFG_NEWFREQ | SYSCTL_RSCLKCFG_USEPLL);
    
         /* Set MOSC is DeepSleep (DSOSCSRC) clock source */
    	 HWREG(SYSCTL_DSCLKCFG) |= SYSCTL_RSCLKCFG_USEPLL;

  • BTW: That open statement of register 10 text contradicts with the later register programming text and note NOXTAL.
  • Hi Chuck,

    Is this launch pad unrecoverable from that seemingly safe register bit change? Seems otherwise the NOXTAL bit if so destructive must be a locked pin like NMI or JTAG pins. The only other possibility is the 25Mhz XTAL was earlier stressed by scope probe on C44.

    Can you please verify report to forum if a single register write clearing (PWRDWN | NOXTAL) bits is an EK-TM4C1294-XL launch pad killer?

    Thank you!
  • Hello BP,

    I am doing some checking on it and will get back with you in a short while. Seems it shouldn't be so catastrophic and that there should be a way to break through it to get the device unlocked and usable again. I'll get back to you in a short while.

  • Hello BP101

    The absence of a MOSC or setting of the MOSC with NO_XTAL should not affect the erase or unlock. After unlock/erase the ROM boot loader will execute and cause the MOSC to start up.
  • Hi Amit,

    Yet right after adding NOXTAL single write the MOSC went silent. LM flash runs through the unlock procedure no error returned, yet MOSC remains silent C4,C45=(12pf) produces no frequency gain.
  • Hello BP101

    I have two simple experiments for you to perform

    1. If you use the MOSC then does it start?
    2. If the flash is erased and the device is power cycled, then does the USB show up as a DFU class device?
  • Hi Amit,

    Seems I was not doing the unlock procedure correctly all these years. Though my way did unlock the DAP every time it seems actually removing USB power while holding reset was key.

    I took that message to mean figuratively after releasing reset to power board as any flash firmware updates DELL servers always left power cycle for the very last step.
  • Hello BP101

    Well that explains a lot of the issues with unlocking sequence. Hence the emphasis in the JTAG application note on the procedure.
  • BP101 said:
    as any flash firmware updates DELL servers

    One wonders if anyone else (EVER) would come to that conclusion?

  • The real ? is how did Unlock clear the user registers and flash and long believed the DAP? Seems the extra step is doing something more on the JTAG interface.

    Many others this forum have been locked out and likely was doing the same procedure below.

    Click on OK first informative message about holding reset need to power device. Then hold the MCU reset click OK to (unlock) click ok again then power cycle board. Power cycle in any device firmware update is always done last not first. Cisco, Dell, HP/Compaq, IBM and other industry leaders. Besides the message is vague and should say something more like:

    "It is necessary to FIRST hold MCU reset button while power cycling the ICDI before clicking this OK button." LOL

    On another note the launch pad has 2 USB ports to supply power and JP3 was set to OTG supplying power via USB hub. I had moved JP3 to ICDI position but wonder how the latter might effect the unlock procedure.