Other Parts Discussed in Thread: TM4C123GH6PZ
I am using CCSV6 (version 6.2.0.00048 on Windows 10 - 64bit) to connect to a Tiva TM4C123GH6PZ microprocessor on a custom board. The board/processor have functioned correctly using a different PC in CCSV5.
Attempting to launch the target configuration independent of any project is successful, however I am unable to connect to the CORTEX_M4_0 core. When I attempt the connection, I receive an Error 1170 message (below). If I attempt to connect to the CS_DAP_0 debug core the connection is successful, however memory map is unable to display values (only displays question marks).
I have attempted:
- Power cycling the board,
- Rebooting the computer,
- Changing USB ports that the XDS200 is plugged in on (does not work on any of the 3 USB3.0 ports available),
- Reducing the TCLK frequency (initally 10.0MHz, then 1.0MHz, 100KHz, 50KHz).
Thank you in advance for any advice you can offer. :)
The error message reads:
Error connecting to the target:
(Error -1170 @ 0x0)
Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK).
(Emulation package 6.0.407.3)
The results of the JTAG connection test all pass:
[Start: Texas Instruments XDS2xx USB Debug Probe]
Execute the command:
%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
C:\Users\AIRSHO~1\AppData\Local\TEXASI~1\
CCS\ti\0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 560/2xx-class product.
This utility will load the program 'xds2xxu.out'.
The library build date was 'Jul 27 2016'.
The library build time was '17:54:51'.
The library package version is '6.0.407.3'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.
The controller has a version number of '13' (0x0000000d).
The controller has an insertion length of '0' (0x00000000).
This utility will attempt to reset the controller.
This utility has successfully reset the controller.
-----[Print the reset-command hardware log-file]-----------------------------
This emulator does not create a reset log-file.
-----[Perform the Integrity scan-test on the JTAG IR]------------------------
This test will use blocks of 64 32-bit words.
This test will be applied just once.
Do a test using 0xFFFFFFFF.
Scan tests: 1, skipped: 0, failed: 0
Do a test using 0x00000000.
Scan tests: 2, skipped: 0, failed: 0
Do a test using 0xFE03E0E2.
Scan tests: 3, skipped: 0, failed: 0
Do a test using 0x01FC1F1D.
Scan tests: 4, skipped: 0, failed: 0
Do a test using 0x5533CCAA.
Scan tests: 5, skipped: 0, failed: 0
Do a test using 0xAACC3355.
Scan tests: 6, skipped: 0, failed: 0
All of the values were scanned correctly.
The JTAG IR Integrity scan-test has succeeded.
-----[Perform the Integrity scan-test on the JTAG DR]------------------------
This test will use blocks of 64 32-bit words.
This test will be applied just once.
Do a test using 0xFFFFFFFF.
Scan tests: 1, skipped: 0, failed: 0
Do a test using 0x00000000.
Scan tests: 2, skipped: 0, failed: 0
Do a test using 0xFE03E0E2.
Scan tests: 3, skipped: 0, failed: 0
Do a test using 0x01FC1F1D.
Scan tests: 4, skipped: 0, failed: 0
Do a test using 0x5533CCAA.
Scan tests: 5, skipped: 0, failed: 0
Do a test using 0xAACC3355.
Scan tests: 6, skipped: 0, failed: 0
All of the values were scanned correctly.
The JTAG DR Integrity scan-test has succeeded.
[End: Texas Instruments XDS2xx USB Debug Probe]
The confugration's CCXML file is as follows:
<?xml version="1.0" encoding="UTF-8" standalone="no"?>
<configurations XML_version="1.2" id="configurations_0">
<configuration XML_version="1.2" id="configuration_0">
<instance XML_version="1.2" desc="Texas Instruments XDS2xx USB Debug Probe" href="connections/TIXDS2XXUSB_Connection.xml" id="Texas Instruments XDS2xx USB Debug Probe" xml="TIXDS2XXUSB_Connection.xml" xmlpath="connections"/>
<connection XML_version="1.2" id="Texas Instruments XDS2xx USB Debug Probe">
<instance XML_version="1.2" href="drivers/tixds560cs_dap.xml" id="drivers" xml="tixds560cs_dap.xml" xmlpath="drivers"/>
<instance XML_version="1.2" href="drivers/tixds560cortexM.xml" id="drivers" xml="tixds560cortexM.xml" xmlpath="drivers"/>
<property Type="choicelist" Value="0" id="The JTAG TCLK Frequency (MHz)">
<choice Name="Fixed with user specified faster value" value="SPECIFIC">
<property Type="stringfield" Value="10.0MHz" id="-- Enter a value from 0.5MHz to 20.0MHz"/>
</choice>
<choice Name="Adaptive with user specified limit" value="ADAPTIVE">
<property Type="stringfield" Value="10.0MHz" id="-- Enter a value from 0.5MHz to 20.0MHz"/>
</choice>
</property>
<platform XML_version="1.2" id="platform_0">
<instance XML_version="1.2" desc="Tiva TM4C123GH6PZ" href="devices/tm4c123gh6pz.xml" id="Tiva TM4C123GH6PZ" xml="tm4c123gh6pz.xml" xmlpath="devices"/>
<device HW_revision="1" XML_version="1.2" description="" id="Tiva TM4C123GH6PZ" partnum="TM4C123GH6PZ" simulation="no">
<router HW_revision="1.0" XML_version="1.2" description="CS_DAP Router" id="CS_DAP_0" isa="CS_DAP">
<subpath id="subpath_0">
<cpu HW_revision="1.0" XML_version="1.2" desc="CORTEX_M4_0" description="Cortex M4 CPU" deviceSim="false" id="CORTEX_M4_0" isa="CORTEX_M4"/>
</subpath>
</router>
</device>
</platform>
</connection>
</configuration>
</configurations>