Other Parts Discussed in Thread: HALCOGEN
Hello guys,
one short question. i have made a project called "test" in ccs and then i made a project called "test" in halcogen aswell. i made my settings there to use the sci communication and the settings were 9600 baud, 8 data bits, no parity, 2 stop bits.
i made the proper linking of the project (right click on project -> properties -> Build/ARM Compiler/include options and i included the right folder).
Everything was working normally and fine.
Then i recgonized that i need to make some changes in the setting (i had to make 115200 baudrate, 8 data bit, no parity, and 1 stop bit (!!) ). i made it like this:
inside my ccs project is a Halcogen file called "Test.hcg". i opened this, made my changes in the sci3 register as above mentioned and i clicked on generate code again.
Then i closed halcogen and went to ccs again. i clicked on "Project-> Build Project" and suddenly i got over 15 errors. like "sciREG3 is undefined" or "sciBASE_t is undefined" etc. So i dont know what i did wrong and how the project is working again.
thanks for every help!
regards ,
Markus