Other Parts Discussed in Thread: TMS570LS3137-EP
I am reading "TMS570LS3137-EP 16- and 32-Bit RISC Flash Microcontroller (Literature Number: SPNS230D)".
About "Table 6-36. ESM Channel Assignments", I want to know the details.
I want to know the safety function or diagnosis to generate a following ERROR SOURCES.
[ERROR SOURCES]
-----------------------------------------------------------------------------------
DMA - imprecise read error
FMC - correctable error: bus1 and bus2 interfaces
DMA - imprecise write error
FMC - correctable error (EEPROM bank access)
FMC - uncorrectable error (EEPROM bank access)
IOMM - Mux configuration error
Ethernet Controller master interface
FMC - uncorrectable error (address parity on bus1 accesses)
RAM even bank (B0TCM) - uncorrectable error
RAM odd bank (B1TCM) - uncorrectable error
RAM even bank (B0TCM) - ECC uncorrectable error
RAM odd bank (B1TCM) - ECC uncorrectable error
FMC - uncorrectable error: bus1 and bus2 interfaces
-----------------------------------------------------------------------------------
From the "Table 4. Summary of Safety Features and Diagnostics" of the Safety Manual, please tell me the Unique Identifier which generates the above error.