Hi,
I am facing the problem in sensor interface. I have interfaced totally 7 sensors to the ADC channel 1. in which channel 0 and 4 are giving the wrong output (compared with expected value or known value of sensor) . I tried to short it out in different ways
1. along with seven channel I have enabled the channel 8 and connected it to the ground then only channel 4 giving the wrong output. when i used
2.when I used only four channels from 0 to 3 all are working fine.
Please help me to sort out the issue. sometimes after the power on/off the wrong output is switched to different channel.