This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Error while loading the executable to RM46Lx2(launchpad) Unhandled stab entry SEVERE: Encountered a problem loading file:"



Hardware: RM46 launchpad

I have successfully generated the application(sumdiff.elf) for the rm46lx with FREE RTOS using GNU GCC tool-chain.
However, i am having trouble while lodaing the application. I am able to connect to the hardware but am getting  an message "Unhandled stab entry
SEVERE: Encountered a problem loading file:" .

Any tips to get me unblocked would be apprecitated.

C:\ti\ccsv6\ccs_base\scripting\examples\loadti>loadti -c C:\Users\aparajul\ti\CCSTargetConfigurations\RM46Lx.ccxml -x C:\work\rm46HDK\Project1_RM46x\log.xml C:\work\rm46HDK\Project1_RM46x\sumdiff.elf -a -v

***** DSS Generic Loader *****

START: 13:03:13 GMT-0400 (EDT)

Configuring Debug Server for specified target...
Done
TARGET: Texas Instruments XDS110 USB Debug Probe_0
Connecting to target...
CortexR4: GEL Output: Memory Map Setup for Flash @ Address 0x0
testEnv.outFiles: C:\work\rm46HDK\Project1_RM46x\sumdiff.elf
Loading C:\work\rm46HDK\Project1_RM46x\sumdiff.elf
CortexR4: GEL Output: Memory Map Setup for Flash @ Address 0x0 due to System Reset

CortexR4: GEL Output: Memory Map Setup for Flash @ Address 0x0 due to System Reset

SEVERE: CortexR4: GEL: Encountered a problem loading file: C:\work\rm46HDK\Project1_RM46x\sumdiff.elf process_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entry

SEVERE: Encountered a problem loading file: C:\work\rm46HDK\Project1_RM46x\sumdiff.elf
process_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entry
SEVERE: Error loading "C:\work\rm46HDK\Project1_RM46x\sumdiff.elf": Encountered a problem loading file: C:\work\rm46HDK\Project1_RM46x\sumdiff.elf
process_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entry
Error code #4011, C:\work\rm46HDK\Project1_RM46x\sumdiff.elf load failed!
Aborting!
333
END: 13:03:32 GMT-0400 (EDT)