Other Parts Discussed in Thread: HALCOGEN, CCSTUDIO, ENERGYTRACE, MSP430WARE, UNIFLASH
Hardware: RM46 launchpad; using FREE-RTOS port provided by TI and generated halcogen project for FREE-RTOS() with GNU GCC tools
I have successfully generated the application(sumdiff.elf) for the rm46lx with FREE RTOS using GNU GCC tool-chain.
However, i am having trouble while lodaing the application. I am able to connect to the hardware but i am getting an message "Unhandled stab entry
SEVERE: Encountered a problem loading file:" .
IS there something wrong with the generated executable?
snapshot of loadti
C:\ti\ccsv6\ccs_base\scripting\examples\loadti>loadti -c C:\Users\aparajul\ti\CCSTargetConfigurations\RM46Lx.ccxml -x C:\work\rm46HDK\Project1_RM46x\log.xml C:\work\rm46HDK\Project1_RM46x\sumdiff.elf -a -v
***** DSS Generic Loader *****
START: 13:03:13 GMT-0400 (EDT)
Configuring Debug Server for specified target...
Done
TARGET: Texas Instruments XDS110 USB Debug Probe_0
Connecting to target...
CortexR4: GEL Output: Memory Map Setup for Flash @ Address 0x0
testEnv.outFiles: C:\work\rm46HDK\Project1_RM46x\sumdiff.elf
Loading C:\work\rm46HDK\Project1_RM46x\sumdiff.elf
CortexR4: GEL Output: Memory Map Setup for Flash @ Address 0x0 due to System Reset
CortexR4: GEL Output: Memory Map Setup for Flash @ Address 0x0 due to System Reset
SEVERE: CortexR4: GEL: Encountered a problem loading file: C:\work\rm46HDK\Project1_RM46x\sumdiff.elf process_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entry
SEVERE: Encountered a problem loading file: C:\work\rm46HDK\Project1_RM46x\sumdiff.elf
process_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entry
SEVERE: Error loading "C:\work\rm46HDK\Project1_RM46x\sumdiff.elf": Encountered a problem loading file: C:\work\rm46HDK\Project1_RM46x\sumdiff.elf
process_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entryprocess_stab: Unhandled stab entry
Error code #4011, C:\work\rm46HDK\Project1_RM46x\sumdiff.elf load failed!
Aborting!
333
END: 13:03:32 GMT-0400 (EDT)