This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

program protection



Is it possible to retrieve the program stored in the flash

  • The question is a bit vague, but assuming you mean can the binary be retrieved then the answer is yes. That's how verify is done when programming the flash.

    Robert
  • Taking the title of this thread into account, one might assume the question is about readout-protected Flash. That raises the suspicion of activities which are non-legal in many countries.

    However, such a poorly framed question begs for an appropriate answer...

  • Such a "poorly-framed" question may (better) beg for, "better framing."

    Firm/I see poster's "Protection" as his main thrust - and NO! such sub 10 (USD) MCUs have only the most primitive protection against skilled, equipped, determined and resource-laden individuals/groups - who seek the MCU's code.

    Governments & large business - near daily - report breaches.   If the sub 10 (USD) MCU offered protection - would they not flock toward its usage?

    Disrupting JTAG or similar may (maybe) delay a "not too experienced 4th grader" - but offers NO CREDIBLE DETERRENT to those who WANT your code!

  • Firm/I see poster's "Protection" as his main thrust - and NO! such sub 10 (USD) MCUs have only the most primitive protection against skilled, equipped, determined and resource-laden individuals/groups - who seek the MCU's code.

    Didn't want to set the O.P. / anyone on this track. For a decent amount, companies in some eastern countries even offer to do this for you ...

  • Well - if one (really) wanted SECURITY - could not an (unsecured) server be placed w/in a closet - surely we're told that, "Would be Safe!"
  • I gess that would fall into the (broader) category of "security by obscurity"...

  • We're told - while NOT recommended - it IS Gov't sanctioned!
  • Government - the finest, brightest, most honest and altruistic men of the country, that only serve their master, the people. Aren't they ???

    But back to the topic - it seems the O.P. finally lost interest. Either because something not-so-legal was involved, or he realized it was the wrong forum again (like his MSP430 cycle count question here...).

  • Not the first time: You, Robert (and unlikely) moi have chased one away...

    At the moment - two are "holding me up" - one shoe's come off - and I'm being hustled into my limo - (feet dragging) for short trip to my daughter's. (or was this (another) dream sequence...that MSP430 cycle count surely will help...)