Other Parts Discussed in Thread: RM48L952, HALCOGEN
Hi, we are using the Hercules RM48L952 board. We want to map an array to the external SDRAM. We understood that the RM48 part is ARM based. Is this correct? Is it then possible to do as ARM documentation suggests (http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.faqs/1500.html:
The emif/sdram is enabled and in the halcogen sys_link.cmd file is configured to access the sdram as follows
MEMORY
{
VECTORS (X) : origin=0x00000000 length=0x00000020
FLASH0 (RX) : origin=0x00000020 length=0x0017FFE0
FLASH1 (RX) : origin=0x00180000 length=0x00180000
STACKS (RW) : origin=0x08000000 length=0x00000900
RAM (RW) : origin=0x08000900 length=0x0003f700
/* USER CODE BEGIN (2) */
SDRAM (RW) : origin=0x80000000 length=0x00200000
/* USER CODE END */
}
/*----------------------------------------------------------------------------*/
/* Section Configuration */
SECTIONS
{
.intvecs : {} > VECTORS
.text : {} > FLASH0 | FLASH1
.const : {} > FLASH0 | FLASH1
.cinit : {} > FLASH0 | FLASH1
.pinit : {} > FLASH0 | FLASH1
.bss : {} > RAM
.data : {} > RAM
/* USER CODE BEGIN (3) */
.sysmem : {} > SDRAM
/* USER CODE END */
FEE_TEXT_SECTION : {} > FLASH0 | FLASH1
FEE_CONST_SECTION : {} > FLASH0 | FLASH1
FEE_DATA_SECTION : {} > RAM
We created a separate .c file for just the array and we created a scatter.txt file with what was advised below, and we added the --scatter scatter.txt to the linker properties. Will this work or does TI recommend a different approach to mapping variables onto the sdram part on the board??
(copy/paste from arm site)
Mapping variables to specific addresses
Memory mapped registers can be accessed from C in two ways: either by forcing a array or struct variable to a specific address, or by using a pointer to an array or struct (see below for details). Both generate efficient code - it is really down to a matter of personal preference.
-
Forcing struct/array to a specific address
The 'variable' should be declared it in a file on its own. When it is compiled, the object code for this file will only contain data. This data can be placed at a specified address using the ARM scatter-loading mechanism. This is the recommended method for placing all
AREAs (code, data, etc) at required locations in the memory map.-
Create a C source file, for example,
iovar.cwhich contains a declaration of the variable/array/struct, e.g.volatile unsigned short u16_IORegs[20];or
struct{
volatile unsigned reg1;
volatile unsigned reg2;
} mem_mapped_reg; -
Create a scatter-loading description file (called
scatter.txt) containing the following:ALL 0x8000
{
ALL 0x8000
{
* (+RO,+RW,+ZI)
}
}
IO 0x40000000
{
IO 0x40000000
{
iovar.o (+ZI)
}
}The scatter-loading description file must be specified at link time to the linker using the
--scatter scatter.txtcommand line option. This creates two different load regions in your image: 'ALL' and 'IO'. The zero-initialised area fromiovar.o(containing your array) goes into the IO area located at0x40000000. All code (RO) and data areas (RWandZI) from other object files go into the 'ALL' region which starts at0x8000.If you have more than one group of variables (more than one set of memory mapped registers) you would need to define each group of variables as a separate execution region (though they could all lie within a single load region). To do this, each group of variables would need to be defined in a separate module.
The benefit of using a scatter-loading description file is that all the (target-specific) absolute addresses chosen for your devices, code and data are located in one file, making maintenance easy. Furthermore, if you decide to change your memory map (for example, if peripherals are moved), you do not need to rebuild your entire project - you only need to re-link the existing objects.
Alternatively, it is possible to use the
#pragma arm sectionpragma to place the data into a specific section and then use scatter-loading to place that data at an explicit location. For further information, please see the ARM Compiler toolchains Compiler Reference documentation.
-