Other Parts Discussed in Thread: TM4C129XNCZAD
Hi,
We're using a TIVA TM4C129XNCZAD MCU with the TI RTOS version 2_14_00_10 in our project. The SDK that comes with this processor uses a 3.5" Kentec LCD that uses the SSD2119 driver chip. Apparently this chip is being discontinued, and we can't find any LCDs (Kentec or others) in our desired size (2.8") that uses the SSD2119 chip and is actually available to purchase.
Is there another display driver chip that the TI RTOS supports? Hopefully the new driver chip will give us more LCD options to select from.
Any help is appreciated,
Fred