I am reading "TMS570LS31x/21x 16/32-Bit RISC Flash Microcontroller Technical Reference Manual (SPNU499B)".
I want you to inform me about the access specification of the register.
The following register table, there is a description of the WP. However, "LEGEND" in, there is no description of the WP.
Which is right?
| FIQ/IRQ Program Control Register 0 |
| FIQ/IRQ Program Control Register 1 |
| FIQ/IRQ Program Control Register 2 |
| Pending Interrupt Read Location Register 0 |
| Pending Interrupt Read Location Register 1 |
| Pending Interrupt Read Location Register 2 |
| Interrupt Enable Set Register 0 |
| Interrupt Enable Set Register 1 |
| Interrupt Enable Set Register 2 |
| Interrupt Enable Clear Register 0 |
| Interrupt Enable Clear Register 1 |
| Interrupt Enable Clear Register 2 |
| Wake-up Enable Set Register 0 |
| Wake-up Enable Set Register 1 |
| Wake-up Enable Set Register 2 |
| Wake-up Enable Clear Register 0 |
| Wake-up Enable Clear Register 1 |
| Wake-up Enable Clear Register 2 |
|
POM Global Control Register |
| POM Status Register |
| POM Program Region Start Address Register x |