Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Interfacing BMP180 with Tiva TM4C129 via i2c

I'm trying to interface BMP180 with TM4C1294 ncpdt  via i2c protocol. But not able to read the temperature values.

Device Address - 0xEF (read) and 0xEE (write).

Link for BMP180 Datasheet - cdn-shop.adafruit.com/.../BST-BMP180-DS000-09.pdf

Below is the code what i have tried to implement, please any suggestions on the issue. Thanks in advance.

#include <stdarg.h>
#include <stdbool.h>
#include <stdint.h>
#include "inc/hw_i2c.h"
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "inc/hw_gpio.h"
#include "driverlib/i2c.h"
#include "driverlib/sysctl.h"
#include "driverlib/gpio.h"
#include "driverlib/pin_map.h"

#define DEVICE_ADDRESS 0xEF
#define W_DEVICE_ADDRESS 0xEE
#define regADD 0x2E
//#define regADD 0xF//0xF6

void InitI2C0()
{

//enable I2C module 0
SysCtlPeripheralEnable(SYSCTL_PERIPH_I2C0);

//reset module
SysCtlPeripheralReset(SYSCTL_PERIPH_I2C0);

//enable GPIO peripheral that contains I2C 0
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);

// Configure the pin muxing for I2C0 functions on port B2 and B3.
GPIOPinConfigure(GPIO_PB2_I2C0SCL);
GPIOPinConfigure(GPIO_PB3_I2C0SDA);

// Select the I2C function for these pins.
GPIOPinTypeI2CSCL(GPIO_PORTB_BASE, GPIO_PIN_2);
GPIOPinTypeI2C(GPIO_PORTB_BASE, GPIO_PIN_3);

// Enable and initialize the I2C0 master module. Use the system clock for
// the I2C0 module. The last parameter sets the I2C data transfer rate.
// If false the data rate is set to 100kbps and if true the data rate will
// be set to 400kbps.
I2CMasterInitExpClk(I2C0_BASE, SysCtlClockGet(), false);

//clear I2C FIFOs
HWREG(I2C0_BASE + I2C_O_FIFOCTL) = 80008000;
//HWREG(I2C0_BASE + I2C_O_MCR) |= 0x01;

}

uint32_t ReadTemp(uint32_t W_slave_address, uint32_t R_slave_address, uint8_t regadd)
{

//specify that we are writing (a register address) to the
//slave device
I2CMasterSlaveAddrSet(I2C0_BASE, R_slave_address, false);

//specify register to be read
I2CMasterDataPut(I2C0_BASE, regadd);

//send control byte and register address byte to slave device
I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_BURST_SEND_START);

//wait for MCU to finish transaction
while(I2CMasterBusy(I2C0_BASE));

//specify that we are going to read from slave device
I2CMasterSlaveAddrSet(I2C0_BASE, R_slave_address, true);

//send control byte and read from the register we
//specified
I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_SINGLE_RECEIVE);

//wait for MCU to finish transaction
while(I2CMasterBusy(I2C0_BASE));

//return data pulled from the specified register
return I2CMasterDataGet(I2C0_BASE);

}


void main(void)
{

// Set the clocking to run directly from the external crystal/oscillator.
SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_PLL | SYSCTL_OSC_INT | SYSCTL_XTAL_16MHZ);

//initialize I2C module 0
InitI2C0();
uint32_t Data;

Data = ReadTemp(W_DEVICE_ADDRESS, DEVICE_ADDRESS, regADD);
SysCtlDelay(5000);
Data = ReadTemp(W_DEVICE_ADDRESS, DEVICE_ADDRESS, regADD);

while(1)
{

}

}