Hey,
I have a problem about configure PWM. I can't see anything from PC4 output.
Here is my init function:
void PWM_Init(void)
{
unsigned long delay;
SYSCTL_RCGC0_R |= 0x00100000; // SYSCTL_RCGC0_PWM0; // 1) Enable the PWM clock
SYSCTL_RCGC2_R |= SYSCTL_RCGC2_GPIOC; // 2) PortC Clock(PC4-M0PWM6; PWM out)
delay = SYSCTL_RCGC2_R;
GPIO_PORTC_AFSEL_R |= 0x10; // PC4 - Alt. Funct.
GPIO_PORTC_PCTL_R &= ~0x000F0000;
GPIO_PORTC_PCTL_R |= 0x00040000; // M0PWM6
GPIO_PORTC_AMSEL_R &= ~0x10; // Disable analog
GPIO_PORTC_DEN_R |= 0x10; // PF2 Digital enabled
SYSCTL_RCC_R |= SYSCTL_RCC_USEPWMDIV; // Use PWM divider
SYSCTL_RCC_R &= ~SYSCTL_RCC_PWMDIV_M; // clear divider
SYSCTL_RCC_R |= SYSCTL_RCC_PWMDIV_64; // /64 divider
// Module 0 PWM Generator 3
PWM0_3_CTL_R = 0; // disable for config
PWM0_3_GENA_R = 0x0000008C;
PWM0_3_LOAD_R = 0x0000013F; // 80Mhz/16=1,250,000hz / 50 = 25,000 (period, 50hz)
PWM0_3_CMPA_R = 0x0000010F; // 50% duty. (12,500)
PWM0_3_CTL_R = 0x00000001; // enable
PWM0_ENABLE_R = 0x40; // PWM0_ENABLE_R |= PWM_ENABLE_PWM6EN;
}
Thanks for any help.