Other Parts Discussed in Thread: RM46L852
Hello.
I use RM46L852 chip and want to generate IRQ for end transfer from CAN3 RAM to IF3 registers.
I write IF3 Observation register with 0x1F and write IF3UPD12/34 registers to watch for message objects.
Then I write an address of my function in VIM RAM vector 60 for IRQ handler and enable that IRQ by setting bit 28 of REQENASET1.
After generation of CAN packet, I see that IF3OBS = 0x9F1F (and it is correct value, IRQ flag with bit15 = 1, all data, control, mask and ID is transfered from CAN RAM to IF3), but no IRQ is generated. What I need to generate IRQ for IF3? Where is IRQ Enable flag for IF3? Do I need to "enable DMA requests for IF3" by setting DE3 in CTL even if I does not use DMA?
All other IRQs for other peripherals is generated correctly.
Regars, Vitaliy