Other Parts Discussed in Thread: TMS570LS1225, TMS570LC4357
We are porting code from a TMS570LS1225 to the TMS570LC4357. I am connecting the debugger (CCS 6.1.0.00104) via an XDS200 emulator.
When the debugger is paused (or hits a breakpoint) the rti clocks keep running. I have checked the rtiREG1-GCTRL register and the continue-on-suspend bit (bit 15) is not set. The register is set to 3 (both counters enabled)
Is there something else I need to do for the LC4357 ? I can't find any significant difference between the new LC43x code and the old LS12x code