Other Parts Discussed in Thread: HALCOGEN
Hello, we are trying to add CAN communications to the supplied TMS570LS12 foc_encoder_speed solution. I generated a CAN example using HALCogen, and that runs fine on the kit, but when I bring that code into the foc_encoder_speed codeset, it does not work - all I get is frame timing errors on the other end. There does not seem to be any pin muxing that needs to be setup for the CAN, so I suspect a clock setup difference. Comparing the two sets of code, there are some differences, but nothing obvious affecting VCLKA1. Here is my CAN init:
canREG1->CTL = (uint32)0x00000000U
| (uint32)0x00000000U
| (uint32)((uint32)0x00000005U << 10U)
| (uint32)0x00020043U;
canREG1->ES |= 0xFFFFFFFFU;
canREG1->INTMUXx[0U] = 0
canREG1->INTMUXx[1U] = 0;
canREG1->ABOTR = (uint32)0U;
while ((canREG1->IF1STAT & 0x80U) ==0x80U)
{
} /* Wait */
canREG1->IF1MSK = 0xC0000000U | (uint32)((uint32)((uint32)0x000007FFU & (uint32)0x000007FFU) << (uint32)18U);
canREG1->IF1ARB = (uint32)0x80000000U | (uint32)0x00000000U | (uint32)0x20000000U | (uint32)((uint32)((uint32)0x581U & (uint32)0x000007FFU) << (uint32)18U);
canREG1->IF1MCTL = 0x00001080U | (uint32)0x00000000U | (uint32)0x00000000U | (uint32)8U;
canREG1->IF1CMD = (uint8) 0xF8U;
canREG1->IF1NO = 1U;
while ((canREG1->IF2STAT & 0x80U) ==0x80U)
{
} /* Wait */
canREG1->IF2MSK = 0xC0000000U | (uint32)((uint32)((uint32)0x000007FFU & (uint32)0x000007FFU) << (uint32)18U);
canREG1->IF2ARB = (uint32)0x80000000U | (uint32)0x00000000U | (uint32)0x00000000U | (uint32)((uint32)((uint32)0x600U & (uint32)0x000007FFU) << (uint32)18U);
canREG1->IF2MCTL = 0x00001080U | (uint32)0x00000400U | (uint32)0x00000000U | (uint32)8U;
canREG1->IF2CMD = (uint8) 0xF8U;
canREG1->IF2NO = 2U;
while ((canREG1->IF1STAT & 0x80U) ==0x80U)
{
} /* Wait */
canREG1->IF1CMD = 0x87U;
while ((canREG1->IF2STAT & 0x80U) ==0x80U)
{
} /* Wait */
canREG1->IF2CMD = 0x17U;
canREG1->BTR = (uint32)((uint32)0U << 16U) |
(uint32)((uint32)(3U - 1U) << 12U) |
(uint32)((uint32)((5U + 3U) - 1U) << 8U) |
(uint32)((uint32)(3U - 1U) << 6U) |
(uint32)14U;
canREG1->TIOC = (uint32)((uint32)1U << 18U )
| (uint32)((uint32)0U << 17U )
| (uint32)((uint32)0U << 16U )
| (uint32)((uint32)1U << 3U )
| (uint32)((uint32)1U << 2U )
| (uint32)((uint32)1U << 1U );
canREG1->RIOC = (uint32)((uint32)1U << 18U )
| (uint32)((uint32)0U << 17U )
| (uint32)((uint32)0U << 16U )
| (uint32)((uint32)1U << 3U )
| (uint32)((uint32)0U << 2U )
| (uint32)((uint32)0U <<1U );
/** - Leave configuration and initialization mode */
canREG1->CTL &= ~(uint32)(0x00000041U);
Any suggestions on what clock setup changes I would need to make to get CAN up an running?
Thanks,
Chuck