This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LC4357: RTI COMPARE INTERRUPT NOT HANDLED .

Other Parts Discussed in Thread: HALCOGEN

Hello,
I'm a new to the Hercules Launchpads.I wrote a small code to test the ability of the RTI to generate a time base and I'm currently facing a predicament of
an unknown origin.
The RTI generates a compare0 interrupt,as indicated by RTIINTFLAG register (bit 0 is 1), but, apparently, the VIM doesn't handle it .
I've cleared the IRQ bit from CPSR, enabled the channel 2 interrupt from REQENASET0 (in VIM) and enabled the interrupt in RTISETINTENA (RTI).
I'd like to mention that I've made a similar program concerning GIO interrupts ,the only difference was the channel and, of course, enabling the interrupt in the
appropriate GIO register.
I've also used rtiInit() to rule out potential initialization erros.
Would you kindly provide some advice regarding the cause of this ?

[CODE BEGIN]__________________________________
#include "HL_sys_common.h"
#include "HL_RTI.h"

#define rti_base 0xFFFFFC00
#define RTIGCTRL ((volatile uint32 *)rti_base)
#define RTITBCTRL ((volatile uint32 *)(rti_base + 0x04))
#define RTICOMPCTRL ((volatile uint32 *)(rti_base +0x0C))
#define RTIFRC0 ((volatile uint32 *)(rti_base +0x10))
#define RTIUC0 ((volatile uint32 *)(rti_base +0x14))
#define RTICPUC0 ((volatile uint32 *)(rti_base +0x18))
#define RTICOMP0  ((volatile uint32 *)(rti_base +0x50))
#define RTIUDCP0 ((volatile uint32 *)(rti_base +0x54))
#define RTISETINTENA ((volatile uint32 *)(rti_base +0x80))
#define RTIINTFLAG ((volatile uint32 *)(rti_base +0x88))
#define RTIINTCLRENABLE ((volatile uint32 *)(rti_base +0xAC))

#define vim_base 0xFFFFFE00
#define IRQINDEX ((volatile uint32 *)(vim_base))
#define FIRQPR0 ((volatile uint32 *)(vim_base+ 0x10))
#define INTREQ0 ((volatile uint32 *)(vim_base+ 0x20))
#define REQENASET0 ((volatile uint32 *)(vim_base+ 0x30))
#define IRQVECREG ((volatile uint32 *)(vim_base+ 0x70))
#define CHANCTRL2 (((volatile uint32 *)(vim_base + 0x80))
#define CHNADDR2 ((volatile uint32 *) (0xFFF8200C))

void THIS_ISR();
volatile uint32 x=0;
volatile uint32 value=0x1000;


void main(void)
{
	//-----------------------------------VIM
 	asm(" MRS R1, CPSR ");			// 
 	asm(" BIC R1, R1 ,#0x80 ");		//  ENABLE IRQ
 	asm(" MSR cpsr_c, r1 ");		//  
 	
	*FIRQPR0 &=(uint32) 0xFFFFFFFB;		
	*REQENASET0 |=(uint32) 0x04;
	*CHNADDR2 =(uint32)  (& THIS_ISR);


	//-----------------------------------RTI
	rtiInit();
	*RTIGCTRL =(uint32) 0x10000;	
	*RTITBCTRL =(uint32) 0;
 	*RTICOMPCTRL |=(uint32) 0x1110;
 	*RTICPUC0 =(uint32) value;
 	*RTIUDCP0=(uint32) 0x40000;
 	*RTICOMP0=(uint32) 0x40000;
 	*RTISETINTENA |=(uint32) 0x100;
 	*RTIINTCLRENABLE &=(uint32) ~(0x01);
 	*RTIGCTRL |=(uint32) 1;
}



void THIS_ISR(){
x++;
asm(" MRS R1, CPSR ");
asm(" BIC R1, R1 ,#0x80 ");
asm(" MSR cpsr_c, r1 ");
}

[CODE END]____________________________________________

Thank you for your time!

  • Hi,

    There's a lot of potential issues with the code above. Generally inserting inline asm statements is frowned upon for starters.
    Also unlike cortex M, on cortex R interrupt handlers are treated differently by the compiler than regular subroutines.
    Those are just two issues.

    I think the best way for you to proceed is to start with the HalCoGen example "example_rtiBlinky.c".
    This will get you up and running to blink an LED w. RTI and through the ISR using HalCoGen' s framework instead of having to create
    the ISR yourself.
  • Hello,

    Thank you for the advice. I will try to tackle this predicament by employing the use of HalCoGen's framework.