This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Hercules RM57Lx lwip performance



What is the max throughput that can be achieved on the TCP with the lwip stack ?  The two R5 cores is not required to run in lock step.

  • Sreekumar,

    As far as I know this isn't something we've measured and the lwIP stack example we have is only demo-ware.
    You would need to measure it yourself. I can tell you that the choice of memory for your packet buffers will impact throughput just based on how the silicon works. [for example, placing the pbuf in slow async SRAM will cause problems if you are trying to sustain 100Mbps etherent throughput].

    BTW the RM57L is a lockstep device (L) and the cores only operate in lockstep. They cannot unlock.