Other Parts Discussed in Thread: TM4C129ENCPDT
Hello,
in our projects we usually use the Lauterbach Trace32 tools for debugging. Now we have a project where we use a TM4C129ENCPDT and develop the code on CCS 6.1 and the TI Compiler (not GCC).
Lauterbach offers a plugin for Eclipse (see http://www2.lauterbach.com/pdf/int_eclipse_gdb.pdf ) which also seems to work in CCS - at least it can be installed without any problems.
To setup the according debug configuration one has to specifiy the path to a GDB debugger executable (see page 9, step 6 in the above document). In GCC there is 'arm-none-eabi-gdb.exe' which would do this task. To me it seems that there is no such executable included in the TI compiler. Or am I missing or misunderstanding anything?
Best regards,
Michael