This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

how to use uniflash?

Other Parts Discussed in Thread: TCI6630K2L, UNIFLASH

I have the following board:

TCIEVMK2LX

SOC: TCI6630K2L

I want to re-flash the flash memory of Stellaris LM3S2D93 by uniflish. I installed the uniflash package available for Linux by uniflash.4.0.97:

root@am:/opt/ti/uniflash_4.0# ./dslite.sh -c /root/workspace_v6_1_3/ks2evm-bmc-post_v1.1.0.6/ks2evm-bmc-post_v1.1.0.6/ks2evm-bmc/bmc/evmks2/K2L/Stellaris\ LM3S2D93.ccxml -p
Executing the following command:
> /opt/ti/uniflash_4.0/deskdb/content/TICloudAgent/linux/ccs_base/DebugServer/bin/DSLite flash -c /root/workspace_v6_1_3/ks2evm-bmc-post_v1.1.0.6/ks2evm-bmc-post_v1.1.0.6/ks2evm-bmc/bmc/evmks2/K2L/Stellaris LM3S2D93.ccxml -p

Failed: Cannot read System Setup data from XML file /root/workspace_v6_1_3/ks2evm-bmc-post_v1.1.0.6/ks2evm-bmc-post_v1.1.0.6/ks2evm-bmc/bmc/evmks2/K2L/Stellaris
Error parsing file:
Fatal Error at (0, 0): An exception occurred! Type:RuntimeException, Message:The primary document entity could not be opened. Id=/root/workspace_v6_1_3/ks2evm-bmc-post_v1.1.0.6/ks2evm-bmc-post_v1.1.0.6/ks2evm-bmc/bmc/evmks2/K2L/Stellaris

How I can use uniflash?

meanwhile the following web page :speaks about uniflash program. there is no such a program......