This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Herculs RM46x launchpad i2c pins confusion.

I just received my Herculus RM46x Launchpad. In the quick user guide it  is shown that i2c pins are at N2HET1[4], N2HET1[9] and N2HET1[24],N2HET1[26].  but RM46L852 16- and 32-Bit RISC Flash Microcontroller (Rev. C)  documentation shows that the pins are at N2HET1[27], N2HET1[29]. And also i am using Halcogen 04.06.00 and it also have the same N2HET1[27], N2HET1[29] i2c PINMUX. so in this case what should i do?

User Guide.

Doccumentation: