Hello ,
I have an IMU with a slave address of 0x20.
it has different register addresses from where we can get 8 bit of data e.g 0x08,0x10,0x12 .
I Succeeded in doing i2c communication between TI TM4C123. But now i have to do communcation between Rm46x and this IMU.
I am a bit confused with the example given in the halcogen. i am following the example something like this. I just want to read 8 bit of data from register address of 0x08.
#include "sys_common.h"
#include "i2c.h"
#define Slave_Address 0x20
#define Slave_Register_address 0x08
#define DATA_COUNT 8
uint8_t RX_Data_Master[8] = { 0 };
void main(void)
{
int repeat = 0; int delay =0;
i2cInit();
/