Other Parts Discussed in Thread: EK-TM4C129EXL, CC3100, EK-TM4C1294XL, UNIFLASH, CC3200
I am attempting to get the cc3100_http_server app running on the EK-TM4C129EXL demo board connected to a CC3100 module booster pack.
This example is located in the tivaware c 2.1.3.156 examples under the TM4C1294xl-boost-cc3100 board.
The example compiles, but an error is encountered when attempting to write the new CC3100 image.
Press and hold USR_SW1 during reset to upload webpages to CC3100
Boosterpack's Serial Flash.
Webpages will be uploaded to CC3100 Boosterpack's Serial Flash.
CC3100 is configured in default state.
CC3100 is configured in AP mode
Uploading webpages to Serial Flash on CC3100 BP.
Opening file www/404.htm
Writing 303 bytes
Opening file www/about.htm
Writing 1834 bytes
Opening file www/block.htm
Writing 511 bytes
Opening file www/block.jpg
Writing 180251 bytes
Opening file www/ek-tm4c1294xl.jpg
Error in creating the file