Other Parts Discussed in Thread: HALCOGEN
Hello,
I am hoping for some clarifying information on ADC Calibration and Offset Error Correction section 22.2.6.1.2 in the RM57 technical reference.
It mentions Computing the error correction value in step 7, but never mentions what computing actually is. I see halcogen just takes the sum of all the values and divides by the number of values (4). Is this the correct calculation?
/* Compute the Offset error correction value */
conv_val[4U]=conv_val[0U]+ conv_val[1U] + conv_val[2U] + conv_val[3U];
conv_val[4U]=(conv_val[4U]/4U);
Thanks!