This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

External interrupt of TM4C123GH6PM launchpad.

Other Parts Discussed in Thread: TM4C123GH6PM

I am using  external interrupt of TM4C123GH6PM launchpad.  I am using square wave to start the external interrupt in PIN PA2. If frequency of the square wave  is 1 Hz the interrupt works well, but if I increase the frequency for 10 Hz or 100 Hz the interrupt no work. Which pin should I use to high frequency?

Thanks