This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Self Test and Calibration for the ADC on the RM57

Is there a sequencing requirement that is Missing from the Technical Reference? Can Self-Test be performed after Calibration or does it need to be performed before? Does self-test effect the Calibration values at all as well? Should Calibration be re-run after self-test?