This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

watchdog timer problem

I'm using watchdog to create watchdog interrupt after 1 sec. delay but watchdog interrupt is not firing .

Im doing following steps:

WATCHDOG1_LOCK_R = 0x1ACCE551;            //unlock watchdog

WATCHDOG1_LOAD_R = 4000000;                    //load value for 250ms delay
while(WATCHDOG1_CTL_R & 0x80000000);   //wait for WRC bit to set
WATCHDOG1_CTL_R = 0x01;

on debug i found that while checking WRC bit it is getting hang in while loop.

why it is happening.? please help.

Thanks,

Dheeraj