This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I would like to recover ( restore) non-volatile registers on Tiva MCU ( the reason is to re-programming "BOOTCFG" register),
so I read the recover sequence
on the chapter "4.3.4.3 Recovering a "Locked" Microcontroller" in the document
"Tiva™ TM4C123GH6PM Microcontroller DATA SHEET",
but I feel the sequence is complex...
Is there any method to recover non-volatile registers , for example , by using any TI tool ?
I would appreciate if someone could reply.
Regards,
Hiroyasu
Hello Amit Ashara,
Thank you for your reply.
I could execute the "Recover the Tiva Mcu" by using Uniflash command.
(And it could be done easily, not complexed.)
And ,I programmed the "Bootcfg" register as I expected.
But the program cound not be configured after power-up.
The value of the Bootcfg register is shown on the attached figure.
And I also attached the CCS project that I used to try to boot.
The CCS Version is 6.1.3.00034.
And, the boot sequence I expected is :demo_primitive.zip
Check the "PB4" port if its polarity is 1 or not.
->
The polarity on the circuit is "0",so the polarity is
unmatched, then check the address *0000 0004.
->
The value of *0000 0004 is "0000 0A9D", so
the Tiva mcu starts to run application program.
And this demo program would be executed ,if I use
CCS and the debugger (XDS100V2),load the program on CCS,
and execute "Run" on CCS.
I wonder what is incorrect about this demo program and the
custom board ( or the setting of "Bootcfg" ?).
What should I do to boot the demo program correctly ?
I would appriciate if someone could reply to my quesiton.
Regards,
Hiroyasu
Hiroyasu Matsubara said:I would appriciate if someone could reply to my quesiton.
Pardon but vendor's Amit has been "all over" your questionS!
Your "appreciation" would better register here if you'd avoid such unfair characterizations. (and surely - NOT in your best interest to be so negative!)