I’m trying to find out what the max sink/source current is for the Hercules processors GPIO ports. If an output is driving high on the Hercules and I ground it low externally, will that damage the port. Or are they current limited with a 1.5k on their outputs? And vice versa, when they are low can I pull them high without damage. The datasheet implies that there is a 1.5k current limiter on there i/o pins.