Other Parts Discussed in Thread: TDC7200EVM
Hi
I have recently purchased the TI TDC7200EVM which can measure the difference in time between
two events with 55 picosecond accuracy. The evaluation board has two banks of pairs of connectors
(ie two double rows) each row is 10 pins long so 40 pins total. The two TIVAs I have TM4C123 and the TM4C1294
have exactly matching female connectors and the 7200 fits exactly - there are also two pins marked on
the 7200 for GND and 3.3V which match exactly the GND and 3.3v of each of the TIVAs. Ive searched to
see if anyone has put the 7200 on the back of one of these TIVAs - the 7200 is designed to work with the MSP430
Q: Does it make sense to get it to work with a TIVA?
cheers, Tim