I am commanding a temperature conversion on TMP570LC4357 revB temperature sensor on the ADC1 pin 31. I am also commanding concurrent conversions on ADC1 (three groups) and ADC2 (three groups), and the resulting ADC value is causing the temperature to read low. As in reading 1134 instead of 1336 as the result of ADC 1 pin 31.
Is it possible that this is related to errata ADC#1? Is it possible that the conversions on ADC2 or other ADC1 groups is impacting ADC1 pin 31 (temperature sensor)?