Other Parts Discussed in Thread: TMS570LS20216
We are considering using this part because of its multiple eCAP inputs and smaller footprint. We want to be sure that we have 100% certainty that the PLL errata will not affect our operation.
1. It appears from the errata and forum discussions that the software errata workaround is not 100% effective. True?
2. It appears from the forum discussions that if we do not setup the PLL and use a direct oscillator-to-GCLK path, that we will not be subject to the errata. True?
3. Is this errata expected to be corrected any time soon, or no?
4. Should we be looking at another TI MCU to get the eCAPs (4 inputs minimum are needed)? We are doing minimal processing and I/O, but the input capture hardware, and flash and RAM ECC are very important to us.
Thanks!