This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UART OverFlow Issue

Hey Forum,

My issue is with using the UART output to the putty terminal. I was attempting to mimic the output of the demo sensorHub code displayed below....

 I was trying to use the same format to display data from my own project (DIY Segway) but i was running into some issues. I have configured my UART the same but my output is not as near to the example. My output is shown below......

 The value options repeat and then i believe my uart is overflowed with information. So what im am trying to achieve is a way to demonstrate my data without the UART constantly repeating the variable names and only updating the variable number.

I have my code attached below and i have posted the sensor hub demo code as well.

MY CODE:

void initUart()
{
	SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
	SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
	GPIOPinConfigure(GPIO_PA0_U0RX);
	GPIOPinConfigure(GPIO_PA1_U0TX);
	GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
	UARTClockSourceSet(UART0_BASE, UART_CLOCK_PIOSC);
	UARTStdioConfig(0, 115200, 16000000);
}

void outputData(int LeftPWM, int RightPWM, int turningVal, int timeVal, int finalMotorVal,int pitchVal, int pitchDeci)
{

    UARTprintf("\033[2J\033[H");
    UARTprintf("Segway Interface Value Monitor\n\n");
    UARTprintf("Pitch Angle\033[31G|\n\n");//accel
    UARTprintf("Left PWM\033[31G Right PWM\n\n");//[54G|
    UARTprintf("Turning Value\033[31G|\n\n");
    UARTprintf("Final Motor Value\033[31G|\n\n");
    UARTprintf("Time Value\033[31G|\n\n");

	g_ui32PrintSkipCounter++;
	if(g_ui32PrintSkipCounter >= PRINT_SKIP_COUNT)
	{
		//
		// Reset skip counter.
		//
		g_ui32PrintSkipCounter = 0;

        UARTprintf("\033[5;17H%3d.%03d", pitchVal, pitchDeci);
        UARTprintf("\033[7;17H%3d %3d", LeftPWM, RightPWM);
        UARTprintf("\033[9;17H%3d", turningVal);
        UARTprintf("\033[19;14H%3d", finalMotorVal);
        UARTprintf("\033[19;17H%3d", timeVal);

	}

}

SENSORHUB CODE:

//*****************************************************************************
//
// compdcm_mpu9150.c - Example use of the SensorLib with the MPU9150
//
// Copyright (c) 2013-2015 Texas Instruments Incorporated.  All rights reserved.
// Software License Agreement
// 
// Texas Instruments (TI) is supplying this software for use solely and
// exclusively on TI's microcontroller products. The software is owned by
// TI and/or its suppliers, and is protected under applicable copyright
// laws. You may not combine this software with "viral" open-source
// software in order to form a larger program.
// 
// THIS SOFTWARE IS PROVIDED "AS IS" AND WITH ALL FAULTS.
// NO WARRANTIES, WHETHER EXPRESS, IMPLIED OR STATUTORY, INCLUDING, BUT
// NOT LIMITED TO, IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE APPLY TO THIS SOFTWARE. TI SHALL NOT, UNDER ANY
// CIRCUMSTANCES, BE LIABLE FOR SPECIAL, INCIDENTAL, OR CONSEQUENTIAL
// DAMAGES, FOR ANY REASON WHATSOEVER.
// 
// This is part of revision 2.1.2.111 of the EK-TM4C123GXL Firmware Package.
//
//*****************************************************************************

#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_memmap.h"
#include "inc/hw_ints.h"
#include "driverlib/debug.h"
#include "driverlib/gpio.h"
#include "driverlib/interrupt.h"
#include "driverlib/pin_map.h"
#include "driverlib/rom.h"
#include "driverlib/sysctl.h"
#include "driverlib/uart.h"
#include "utils/uartstdio.h"
#include "sensorlib/hw_mpu9150.h"
#include "sensorlib/hw_ak8975.h"
#include "sensorlib/i2cm_drv.h"
#include "sensorlib/ak8975.h"
#include "sensorlib/mpu9150.h"
#include "sensorlib/comp_dcm.h"
#include "drivers/rgb.h"

//*****************************************************************************
//
//! \addtogroup example_list
//! <h1>Nine Axis Sensor Fusion with the MPU9150 and Complimentary-Filtered
//! DCM (compdcm_mpu9150)</h1>
//!
//! This example demonstrates the basic use of the Sensor Library, TM4C123G
//! LaunchPad and SensHub BoosterPack to obtain nine axis motion measurements
//! from the MPU9150.  The example fuses the nine axis measurements into a set
//! of Euler angles: roll, pitch and yaw.  It also produces the rotation
//! quaternions.  The fusion mechanism demonstrated is complimentary-filtered
//! direct cosine matrix (DCM) algorithm is provided as part of the Sensor
//! Library.
//!
//! Connect a serial terminal program to the LaunchPad's ICDI virtual serial
//! port at 115,200 baud.  Use eight bits per byte, no parity and one stop bit.
//! The raw sensor measurements, Euler angles and quaternions are printed to
//! the terminal.  The RGB LED begins to blink at 1Hz after initialization is
//! completed and the example application is running.
//
//*****************************************************************************

//*****************************************************************************
//
// Define MPU9150 I2C Address.
//
//*****************************************************************************
#define MPU9150_I2C_ADDRESS     0x68

//*****************************************************************************
//
// Global array for holding the color values for the RGB.
//
//*****************************************************************************
uint32_t g_pui32Colors[3];

//*****************************************************************************
//
// Global instance structure for the I2C master driver.
//
//*****************************************************************************
tI2CMInstance g_sI2CInst;

//*****************************************************************************
//
// Global instance structure for the ISL29023 sensor driver.
//
//*****************************************************************************
tMPU9150 g_sMPU9150Inst;

//*****************************************************************************
//
// Global Instance structure to manage the DCM state.
//
//*****************************************************************************
tCompDCM g_sCompDCMInst;

//*****************************************************************************
//
// Global flags to alert main that MPU9150 I2C transaction is complete
//
//*****************************************************************************
volatile uint_fast8_t g_vui8I2CDoneFlag;

//*****************************************************************************
//
// Global flags to alert main that MPU9150 I2C transaction error has occurred.
//
//*****************************************************************************
volatile uint_fast8_t g_vui8ErrorFlag;

//*****************************************************************************
//
// Global flags to alert main that MPU9150 data is ready to be retrieved.
//
//*****************************************************************************
volatile uint_fast8_t g_vui8DataFlag;

//*****************************************************************************
//
// Global counter to control and slow down the rate of data to the terminal.
//
//*****************************************************************************
#define PRINT_SKIP_COUNT        10

uint32_t g_ui32PrintSkipCounter;

//*****************************************************************************
//
// The error routine that is called if the driver library encounters an error.
//
//*****************************************************************************
#ifdef DEBUG
void
__error__(char *pcFilename, uint32_t ui32Line)
{
}
#endif

//*****************************************************************************
//
// MPU9150 Sensor callback function.  Called at the end of MPU9150 sensor
// driver transactions. This is called from I2C interrupt context. Therefore,
// we just set a flag and let main do the bulk of the computations and display.
//
//*****************************************************************************
void
MPU9150AppCallback(void *pvCallbackData, uint_fast8_t ui8Status)
{
    //
    // If the transaction succeeded set the data flag to indicate to
    // application that this transaction is complete and data may be ready.
    //
    if(ui8Status == I2CM_STATUS_SUCCESS)
    {
        g_vui8I2CDoneFlag = 1;
    }

    //
    // Store the most recent status in case it was an error condition
    //
    g_vui8ErrorFlag = ui8Status;
}

//*****************************************************************************
//
// Called by the NVIC as a result of GPIO port B interrupt event. For this
// application GPIO port B pin 2 is the interrupt line for the MPU9150
//
//*****************************************************************************
void
IntGPIOb(void)
{
    unsigned long ulStatus;

    ulStatus = GPIOIntStatus(GPIO_PORTB_BASE, true);

    //
    // Clear all the pin interrupts that are set
    //
    GPIOIntClear(GPIO_PORTB_BASE, ulStatus);

    if(ulStatus & GPIO_PIN_2)
    {
        //
        // MPU9150 Data is ready for retrieval and processing.
        //
        MPU9150DataRead(&g_sMPU9150Inst, MPU9150AppCallback, &g_sMPU9150Inst);
    }
}

//*****************************************************************************
//
// Called by the NVIC as a result of I2C3 Interrupt. I2C3 is the I2C connection
// to the MPU9150.
//
//*****************************************************************************
void
MPU9150I2CIntHandler(void)
{
    //
    // Pass through to the I2CM interrupt handler provided by sensor library.
    // This is required to be at application level so that I2CMIntHandler can
    // receive the instance structure pointer as an argument.
    //
    I2CMIntHandler(&g_sI2CInst);
}

//*****************************************************************************
//
// MPU9150 Application error handler. Show the user if we have encountered an
// I2C error.
//
//*****************************************************************************
void
MPU9150AppErrorHandler(char *pcFilename, uint_fast32_t ui32Line)
{
    //
    // Set terminal color to red and print error status and locations
    //
    UARTprintf("\033[31;1m");
    UARTprintf("Error: %d, File: %s, Line: %d\n"
               "See I2C status definitions in sensorlib\\i2cm_drv.h\n",
               g_vui8ErrorFlag, pcFilename, ui32Line);

    //
    // Return terminal color to normal
    //
    UARTprintf("\033[0m");

    //
    // Set RGB Color to RED
    //
    g_pui32Colors[0] = 0xFFFF;
    g_pui32Colors[1] = 0;
    g_pui32Colors[2] = 0;
    RGBColorSet(g_pui32Colors);

    //
    // Increase blink rate to get attention
    //
    RGBBlinkRateSet(10.0f);

    //
    // Go to sleep wait for interventions.  A more robust application could
    // attempt corrective actions here.
    //
    while(1)
    {
        //
        // Do Nothing
        //
    }
}

//*****************************************************************************
//
// Function to wait for the MPU9150 transactions to complete. Use this to spin
// wait on the I2C bus.
//
//*****************************************************************************
void
MPU9150AppI2CWait(char *pcFilename, uint_fast32_t ui32Line)
{
    //
    // Put the processor to sleep while we wait for the I2C driver to
    // indicate that the transaction is complete.
    //
    while((g_vui8I2CDoneFlag == 0) && (g_vui8ErrorFlag == 0))
    {
        //
        // Do Nothing
        //
    }

    //
    // If an error occurred call the error handler immediately.
    //
    if(g_vui8ErrorFlag)
    {
        MPU9150AppErrorHandler(pcFilename, ui32Line);
    }

    //
    // clear the data flag for next use.
    //
    g_vui8I2CDoneFlag = 0;
}

//*****************************************************************************
//
// Configure the UART and its pins.  This must be called before UARTprintf().
//
//*****************************************************************************
void
ConfigureUART(void)
{
    //
    // Enable the GPIO Peripheral used by the UART.
    //
    ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);

    //
    // Enable UART0
    //
    ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);

    //
    // Configure GPIO Pins for UART mode.
    //
    ROM_GPIOPinConfigure(GPIO_PA0_U0RX);
    ROM_GPIOPinConfigure(GPIO_PA1_U0TX);
    ROM_GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);

    //
    // Use the internal 16MHz oscillator as the UART clock source.
    //
    UARTClockSourceSet(UART0_BASE, UART_CLOCK_PIOSC);

    //
    // Initialize the UART for console I/O.
    //
    UARTStdioConfig(0, 115200, 16000000);
}

//*****************************************************************************
//
// Main application entry point.
//
//*****************************************************************************
int
main(void)
{
    int_fast32_t i32IPart[16], i32FPart[16];
    uint_fast32_t ui32Idx, ui32CompDCMStarted;
    float pfData[16];
    float *pfAccel, *pfGyro, *pfMag, *pfEulers, *pfQuaternion;

    //
    // Initialize convenience pointers that clean up and clarify the code
    // meaning. We want all the data in a single contiguous array so that
    // we can make our pretty printing easier later.
    //
    pfAccel = pfData;
    pfGyro = pfData + 3;
    pfMag = pfData + 6;
    pfEulers = pfData + 9;
    pfQuaternion = pfData + 12;

    //
    // Setup the system clock to run at 40 Mhz from PLL with crystal reference
    //
    ROM_SysCtlClockSet(SYSCTL_SYSDIV_5 | SYSCTL_USE_PLL | SYSCTL_XTAL_16MHZ |
                       SYSCTL_OSC_MAIN);

    //
    // Enable port B used for motion interrupt.
    //
    ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);

    //
    // Initialize the UART.
    //
    ConfigureUART();

    //
    // Print the welcome message to the terminal.
    //
    UARTprintf("\033[2JMPU9150 Raw Example\n");

    //
    // Set the color to a purple approximation.
    //
    g_pui32Colors[RED] = 0x8000;
    g_pui32Colors[BLUE] = 0x8000;
    g_pui32Colors[GREEN] = 0x0000;

    //
    // Initialize RGB driver.
    //
    RGBInit(0);
    RGBColorSet(g_pui32Colors);
    RGBIntensitySet(0.5f);
    RGBEnable();

    //
    // The I2C3 peripheral must be enabled before use.
    //
    ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_I2C3);
    ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);

    //
    // Configure the pin muxing for I2C3 functions on port D0 and D1.
    //
    ROM_GPIOPinConfigure(GPIO_PD0_I2C3SCL);
    ROM_GPIOPinConfigure(GPIO_PD1_I2C3SDA);

    //
    // Select the I2C function for these pins.  This function will also
    // configure the GPIO pins pins for I2C operation, setting them to
    // open-drain operation with weak pull-ups.  Consult the data sheet
    // to see which functions are allocated per pin.
    //
    GPIOPinTypeI2CSCL(GPIO_PORTD_BASE, GPIO_PIN_0);
    ROM_GPIOPinTypeI2C(GPIO_PORTD_BASE, GPIO_PIN_1);

    //
    // Configure and Enable the GPIO interrupt. Used for INT signal from the
    // MPU9150
    //
    ROM_GPIOPinTypeGPIOInput(GPIO_PORTB_BASE, GPIO_PIN_2);
    GPIOIntEnable(GPIO_PORTB_BASE, GPIO_PIN_2);
    ROM_GPIOIntTypeSet(GPIO_PORTB_BASE, GPIO_PIN_2, GPIO_FALLING_EDGE);
    ROM_IntEnable(INT_GPIOB);

    //
    // Keep only some parts of the systems running while in sleep mode.
    // GPIOB is for the MPU9150 interrupt pin.
    // UART0 is the virtual serial port
    // TIMER0, TIMER1 and WTIMER5 are used by the RGB driver
    // I2C3 is the I2C interface to the ISL29023
    //
    ROM_SysCtlPeripheralClockGating(true);
    ROM_SysCtlPeripheralSleepEnable(SYSCTL_PERIPH_GPIOB);
    ROM_SysCtlPeripheralSleepEnable(SYSCTL_PERIPH_UART0);
    ROM_SysCtlPeripheralSleepEnable(SYSCTL_PERIPH_TIMER0);
    ROM_SysCtlPeripheralSleepEnable(SYSCTL_PERIPH_TIMER1);
    ROM_SysCtlPeripheralSleepEnable(SYSCTL_PERIPH_I2C3);
    ROM_SysCtlPeripheralSleepEnable(SYSCTL_PERIPH_WTIMER5);

    //
    // Enable interrupts to the processor.
    //
    ROM_IntMasterEnable();

    //
    // Initialize I2C3 peripheral.
    //
    I2CMInit(&g_sI2CInst, I2C3_BASE, INT_I2C3, 0xff, 0xff,
             ROM_SysCtlClockGet());

    //
    // Initialize the MPU9150 Driver.
    //
    MPU9150Init(&g_sMPU9150Inst, &g_sI2CInst, MPU9150_I2C_ADDRESS,
                MPU9150AppCallback, &g_sMPU9150Inst);

    //
    // Wait for transaction to complete
    //
    MPU9150AppI2CWait(__FILE__, __LINE__);

    //
    // Write application specifice sensor configuration such as filter settings
    // and sensor range settings.
    //
    g_sMPU9150Inst.pui8Data[0] = MPU9150_CONFIG_DLPF_CFG_94_98;
    g_sMPU9150Inst.pui8Data[1] = MPU9150_GYRO_CONFIG_FS_SEL_250;
    g_sMPU9150Inst.pui8Data[2] = (MPU9150_ACCEL_CONFIG_ACCEL_HPF_5HZ |
                                  MPU9150_ACCEL_CONFIG_AFS_SEL_2G);
    MPU9150Write(&g_sMPU9150Inst, MPU9150_O_CONFIG, g_sMPU9150Inst.pui8Data, 3,
                 MPU9150AppCallback, &g_sMPU9150Inst);

    //
    // Wait for transaction to complete
    //
    MPU9150AppI2CWait(__FILE__, __LINE__);

    //
    // Configure the data ready interrupt pin output of the MPU9150.
    //
    g_sMPU9150Inst.pui8Data[0] = MPU9150_INT_PIN_CFG_INT_LEVEL |
                                    MPU9150_INT_PIN_CFG_INT_RD_CLEAR |
                                    MPU9150_INT_PIN_CFG_LATCH_INT_EN;
    g_sMPU9150Inst.pui8Data[1] = MPU9150_INT_ENABLE_DATA_RDY_EN;
    MPU9150Write(&g_sMPU9150Inst, MPU9150_O_INT_PIN_CFG,
                 g_sMPU9150Inst.pui8Data, 2, MPU9150AppCallback,
                 &g_sMPU9150Inst);

    //
    // Wait for transaction to complete
    //
    MPU9150AppI2CWait(__FILE__, __LINE__);

    //
    // Initialize the DCM system. 50 hz sample rate.
    // accel weight = .2, gyro weight = .8, mag weight = .2
    //
    CompDCMInit(&g_sCompDCMInst, 1.0f / 50.0f, 0.2f, 0.6f, 0.2f);

    UARTprintf("\033[2J\033[H");
    UARTprintf("MPU9150 9-Axis Simple Data Application Example\n\n");
    UARTprintf("\033[20GX\033[31G|\033[43GY\033[54G|\033[66GZ\n\n");
    UARTprintf("Accel\033[8G|\033[31G|\033[54G|\n\n");
    UARTprintf("Gyro\033[8G|\033[31G|\033[54G|\n\n");
    UARTprintf("Mag\033[8G|\033[31G|\033[54G|\n\n");
    UARTprintf("\n\033[20GRoll\033[31G|\033[43GPitch\033[54G|\033[66GYaw\n\n");
    UARTprintf("Eulers\033[8G|\033[31G|\033[54G|\n\n");

    UARTprintf("\n\033[17GQ1\033[26G|\033[35GQ2\033[44G|\033[53GQ3\033[62G|"
               "\033[71GQ4\n\n");
    UARTprintf("Q\033[8G|\033[26G|\033[44G|\033[62G|\n\n");

    //
    // Enable blinking indicates config finished successfully
    //
    RGBBlinkRateSet(1.0f);

    ui32CompDCMStarted = 0;

    while(1)
    {
        //
        // Go to sleep mode while waiting for data ready.
        //
        while(!g_vui8I2CDoneFlag)
        {
            ROM_SysCtlSleep();
        }

        //
        // Clear the flag
        //
        g_vui8I2CDoneFlag = 0;

        //
        // Get floating point version of the Accel Data in m/s^2.
        //
        MPU9150DataAccelGetFloat(&g_sMPU9150Inst, pfAccel, pfAccel + 1,
                                 pfAccel + 2);

        //
        // Get floating point version of angular velocities in rad/sec
        //
        MPU9150DataGyroGetFloat(&g_sMPU9150Inst, pfGyro, pfGyro + 1,
                                pfGyro + 2);

        //
        // Get floating point version of magnetic fields strength in tesla
        //
        MPU9150DataMagnetoGetFloat(&g_sMPU9150Inst, pfMag, pfMag + 1,
                                   pfMag + 2);

        //
        // Check if this is our first data ever.
        //
        if(ui32CompDCMStarted == 0)
        {
            //
            // Set flag indicating that DCM is started.
            // Perform the seeding of the DCM with the first data set.
            //
            ui32CompDCMStarted = 1;
            CompDCMMagnetoUpdate(&g_sCompDCMInst, pfMag[0], pfMag[1],
                                 pfMag[2]);
            CompDCMAccelUpdate(&g_sCompDCMInst, pfAccel[0], pfAccel[1],
                               pfAccel[2]);
            CompDCMGyroUpdate(&g_sCompDCMInst, pfGyro[0], pfGyro[1],
                              pfGyro[2]);
            CompDCMStart(&g_sCompDCMInst);
        }
        else
        {
            //
            // DCM Is already started.  Perform the incremental update.
            //
            CompDCMMagnetoUpdate(&g_sCompDCMInst, pfMag[0], pfMag[1],
                                 pfMag[2]);
            CompDCMAccelUpdate(&g_sCompDCMInst, pfAccel[0], pfAccel[1],
                               pfAccel[2]);
            CompDCMGyroUpdate(&g_sCompDCMInst, -pfGyro[0], -pfGyro[1],
                              -pfGyro[2]);
            CompDCMUpdate(&g_sCompDCMInst);
        }

        //
        // Increment the skip counter.  Skip counter is used so we do not
        // overflow the UART with data.
        //
        g_ui32PrintSkipCounter++;
        if(g_ui32PrintSkipCounter >= PRINT_SKIP_COUNT)
        {
            //
            // Reset skip counter.
            //
            g_ui32PrintSkipCounter = 0;

            //
            // Get Euler data. (Roll Pitch Yaw)
            //
            CompDCMComputeEulers(&g_sCompDCMInst, pfEulers, pfEulers + 1,
                                 pfEulers + 2);

            //
            // Get Quaternions.
            //
            CompDCMComputeQuaternion(&g_sCompDCMInst, pfQuaternion);

            //
            // convert mag data to micro-tesla for better human interpretation.
            //
            pfMag[0] *= 1e6;
            pfMag[1] *= 1e6;
            pfMag[2] *= 1e6;

            //
            // Convert Eulers to degrees. 180/PI = 57.29...
            // Convert Yaw to 0 to 360 to approximate compass headings.
            //
            pfEulers[0] *= 57.295779513082320876798154814105f;
            pfEulers[1] *= 57.295779513082320876798154814105f;
            pfEulers[2] *= 57.295779513082320876798154814105f;
            if(pfEulers[2] < 0)
            {
                pfEulers[2] += 360.0f;
            }

            //
            // Now drop back to using the data as a single array for the
            // purpose of decomposing the float into a integer part and a
            // fraction (decimal) part.
            //
            for(ui32Idx = 0; ui32Idx < 16; ui32Idx++)
            {
                //
                // Conver float value to a integer truncating the decimal part.
                //
                i32IPart[ui32Idx] = (int32_t) pfData[ui32Idx];

                //
                // Multiply by 1000 to preserve first three decimal values.
                // Truncates at the 3rd decimal place.
                //
                i32FPart[ui32Idx] = (int32_t) (pfData[ui32Idx] * 1000.0f);

                //
                // Subtract off the integer part from this newly formed decimal
                // part.
                //
                i32FPart[ui32Idx] = i32FPart[ui32Idx] -
                                    (i32IPart[ui32Idx] * 1000);

                //
                // make the decimal part a positive number for display.
                //
                if(i32FPart[ui32Idx] < 0)
                {
                    i32FPart[ui32Idx] *= -1;
                }
            }

            //
            // Print the acceleration numbers in the table.
            //
            UARTprintf("\033[5;17H%3d.%03d", i32IPart[0], i32FPart[0]);
            UARTprintf("\033[5;40H%3d.%03d", i32IPart[1], i32FPart[1]);
            UARTprintf("\033[5;63H%3d.%03d", i32IPart[2], i32FPart[2]);

            //
            // Print the angular velocities in the table.
            //
            UARTprintf("\033[7;17H%3d.%03d", i32IPart[3], i32FPart[3]);
            UARTprintf("\033[7;40H%3d.%03d", i32IPart[4], i32FPart[4]);
            UARTprintf("\033[7;63H%3d.%03d", i32IPart[5], i32FPart[5]);

            //
            // Print the magnetic data in the table.
            //
            UARTprintf("\033[9;17H%3d.%03d", i32IPart[6], i32FPart[6]);
            UARTprintf("\033[9;40H%3d.%03d", i32IPart[7], i32FPart[7]);
            UARTprintf("\033[9;63H%3d.%03d", i32IPart[8], i32FPart[8]);

            //
            // Print the Eulers in a table.
            //
           // UARTprintf("\033[14;17H%3d.%03d", i32IPart[9], i32FPart[9]);
            UARTprintf("\033[14;40H%3d.%03d", i32IPart[10], i32FPart[10]);
           // UARTprintf("\033[14;63H%3d.%03d", i32IPart[11], i32FPart[11]);

            //
            // Print the quaternions in a table format.
            //
            UARTprintf("\033[19;17H%3d.%03d", i32IPart[12], i32FPart[12]);
            UARTprintf("\033[19;32H%3d.%03d", i32IPart[13], i32FPart[13]);
            UARTprintf("\033[19;50H%3d.%03d", i32IPart[14], i32FPart[14]);
            UARTprintf("\033[19;68H%3d.%03d", i32IPart[15], i32FPart[15]);

        }
    }
}

I hope my post is clear enough to understand! Please Help!

  • Hello Nelson.

    While I understand the issue you are seeing, I would still like to ask what is the console program you are using when the code is not working?
  • I am using the recommend one from the TIVA C labs with the same steps as well.  PuTTY 

  • Hello Nelson,

    So that we are on the same page, what you want the display to look as is the case of the sensor hub but the values updating in field?

    And right now (1) it is not updating in line and (2) it is printing something not expected?
  • Yes, so same as sensor hub except with different variable names (which i have setup) with the values updating in their fields. And as of right now it is not updating in line and printing unexpected information.
  • Hello Nelson,

    First task is to get the information corrected. Instead of the existing print statements if you print the data as

    UARTprintf("%3d.%03d\n", pitchVal, pitchDeci);
    UARTprintf("%3d %3d\n", LeftPWM, RightPWM);
    UARTprintf("%3d"\n, turningVal);
    UARTprintf("%3d\n", finalMotorVal);
    UARTprintf("%3d\n", timeVal);

    Then does the data come as expected? Please do note to comment out the existing code in the if statement and the function invocation.
  • I tested out the code and i received the same result. I am also passing set values to only test this function.

    Ex.

    outputData(45, 45, 0, 0, 45,45,45);

  • Hello Nelson

    Did you comment out all the UARTprintf before the if statement and then try the same. Also snapshot of the PuTTY log please.
  • Hello Nelson,

    I tried the following attached code in my CCS environment with TeraTerm.  After making some changes to the print statements it is working as expected.

    #include <stdint.h>
    #include <stdbool.h>
    #include "inc/hw_ints.h"
    #include "inc/hw_memmap.h"
    #include "inc/hw_types.h"
    #include "driverlib/debug.h"
    #include "driverlib/gpio.h"
    #include "driverlib/interrupt.h"
    #include "driverlib/pin_map.h"
    #include "driverlib/rom.h"
    #include "driverlib/sysctl.h"
    #include "driverlib/uart.h"
    #include "utils/uartstdio.h"
    
    //*****************************************************************************
    //! UART0, connected to the Virtual Serial Port and running at 115,200, 8-N-1,
    //! is used to display messages from this application.
    //
    //*****************************************************************************
    
    //*****************************************************************************
    //
    // The error routine that is called if the driver library encounters an error.
    //
    //*****************************************************************************
    #ifdef DEBUG
    void
    __error__(char *pcFilename, uint32_t ui32Line)
    {
    }
    #endif
    
    //*****************************************************************************
    //
    // Configure the UART and its pins. This must be called before UARTprintf().
    //
    //*****************************************************************************
    void
    ConfigureUART(void)
    {
    	//
    	// Enable the GPIO Peripheral used by the UART.
    	//
    	ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
    
    	//
    	// Enable UART0
    	//
    	ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
    
    	//
    	// Configure GPIO Pins for UART mode.
    	//
    	ROM_GPIOPinConfigure(GPIO_PA0_U0RX);
    	ROM_GPIOPinConfigure(GPIO_PA1_U0TX);
    	ROM_GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
    
    	//
    	// Use the internal 16MHz oscillator as the UART clock source.
    	//
    	UARTClockSourceSet(UART0_BASE, UART_CLOCK_PIOSC);
    
    	//
    	// Initialize the UART for console I/O.
    	//
    	UARTStdioConfig(0, 115200, 16000000);
    }
    
    void outputData(int LeftPWM, int RightPWM, int turningVal, int timeVal, int finalMotorVal,int pitchVal, int pitchDeci)
    {
    
        UARTprintf("\033[3;24H%3d.%03d", pitchVal, pitchDeci);
        UARTprintf("\033[5;28H%3d \033[5;60H%3d", LeftPWM, RightPWM);
        UARTprintf("\033[7;28H%3d", turningVal);
        UARTprintf("\033[9;28H%3d", finalMotorVal);
        UARTprintf("\033[11;28H%3d", timeVal);
    }
    //*****************************************************************************
    //
    //*****************************************************************************
    int
    main(void)
    {
    	uint8_t ui8Data=0;
    
    	//
    	// System Clock of 50 MHz
    	//
    	ROM_SysCtlClockSet(SYSCTL_SYSDIV_4 | SYSCTL_USE_PLL | SYSCTL_OSC_MAIN |
    			SYSCTL_XTAL_16MHZ);
    
    	//
    	// Initialize the UART and write status.
    	//
    	ConfigureUART();
    
    	UARTprintf("\033[2J\033[H");
    	UARTprintf("Segway Interface Value Monitor\n\n");
    	UARTprintf("Pitch Angle\033[31G|\n\n");//accel
    	UARTprintf("Left PWM\033[31G Right PWM\033[63G\n\n");//[54G|
    	UARTprintf("Turning Value\033[31G|\n\n");
    	UARTprintf("Final Motor Value\033[31G|\n\n");
    	UARTprintf("Time Value\033[31G|\n\n");
    
    
    
    	while(1)
    	{
    		ROM_SysCtlDelay(ROM_SysCtlClockGet()/3);
    		outputData(ui8Data, ui8Data, 0, 0, (ui8Data+1), ui8Data, ui8Data);
    		ui8Data++;
    	}
    }
    

    Hopefully it will work as a reference code for you.

  • Thank you so much! It worked on my end. If you do not mind do you mind explaining why the system delay was needed?
  • Hello Nelson

    Of course. If I had not put the System Delay, I would have been seeing the values updated too fast to debug. You may reduce it as per your requirements or eliminate it.