This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem loading application on the Tiva TM4C129

Hi,

Because the usage of my application, we can only load the application by serial port.  So I tried to use the sflash to reprogram my application by doing "sflash file.bin -c /dev/ttyUSB0 -b 115200 -s 60 -d -p 0x00. However, the screen got stuck at Erasing flash forever. I also try to just ping the UART port by sending 0x03 0x20 0x20 or auto baud rate using 0x55 0x55 and nothing returns back. Did I do anything wrong? If I use LM programmer, it works like magic. What is the difference between the 2 tools? Do I need to condition anything before I use sflash through the UART port?

Thanks

Christy