Hallo
I am a beginner with dma working on tm4c1294XL
I ahve modified the lab14 project so i can get a "one-shot" transfer in the main loop , so i can change the frequency and so on....it works
Code is below
// Lab14a - DMA
#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_ints.h"
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "inc/hw_uart.h"
#include "driverlib/fpu.h"
#include "driverlib/gpio.h"
#include "driverlib/interrupt.h"
#include "driverlib/pin_map.h"
#include "driverlib/rom.h"
#include "driverlib/sysctl.h"
#include "driverlib/udma.h"
uint32_t ui32SysClkFreq;
// Define source and destination buffers
#define MEM_BUFFER_SIZE         1024
static uint32_t g_ui32SrcBuf[MEM_BUFFER_SIZE];
static uint32_t g_ui32DstBuf[MEM_BUFFER_SIZE];
// Define errors counters
static uint32_t g_ui32DMAErrCount = 0;
static uint32_t g_ui32BadISR = 0;
// Define transfer counter
static uint32_t g_ui32MemXferCount = 0;
// The control table used by the uDMA controller.  This table must be aligned to a 1024 byte boundary.
#pragma DATA_ALIGN(pui8ControlTable, 1024)
uint8_t pui8ControlTable[1024];
// uDMA transfer error handler
void uDMAErrorHandler(void) {
	uint32_t ui32Status;
	// Check for uDMA error bit
	ui32Status = uDMAErrorStatusGet();
	// If there is a uDMA error, then clear the error and increment the error counter.
	if (ui32Status) {
		uDMAErrorStatusClear();
		g_ui32DMAErrCount++;
	}
}
// uDMA interrupt handler. Run when transfer is complete.
void uDMAIntHandler(void) {
	uint32_t ui32Mode;
	// Check for the primary control structure to indicate complete.
	ui32Mode = uDMAChannelModeGet(UDMA_CHANNEL_SW);
	if (ui32Mode == UDMA_MODE_STOP) {
		// Increment the count of completed transfers.
		g_ui32MemXferCount++;
		//trasferisci();
	}
	// If the channel is not stopped, then something is wrong.
	else {
		g_ui32BadISR++;
	}
}
// Initialize the uDMA software channel to perform a memory to memory uDMA transfer.
void InitSWTransfer(void) {
	uint32_t ui32Idx;
	// Fill the source memory buffer with a simple incrementing pattern.
	for (ui32Idx = 0; ui32Idx < MEM_BUFFER_SIZE; ui32Idx++) {
		g_ui32SrcBuf[ui32Idx] = ui32Idx;
	}
	// Enable interrupts from the uDMA software channel.
	IntEnable(INT_UDMA);
	// Place the uDMA channel attributes in a known state. These should already be disabled by default.
	uDMAChannelAttributeDisable(UDMA_CHANNEL_SW,
			UDMA_ATTR_USEBURST | UDMA_ATTR_ALTSELECT
					| (UDMA_ATTR_HIGH_PRIORITY | UDMA_ATTR_REQMASK));
	// Configure the control parameters for the SW channel.  The SW channel
	// will be used to transfer between two memory buffers, 32 bits at a time,
	// and the address increment is 32 bits for both source and destination.
	// The arbitration size will be set to 8, which causes the uDMA controller
	// to rearbitrate after 8 items are transferred.  This keeps this channel from
	// hogging the uDMA controller once the transfer is started, and allows other
	// channels to get serviced if they are higher priority.
	uDMAChannelControlSet(UDMA_CHANNEL_SW | UDMA_PRI_SELECT,
			UDMA_SIZE_32 | UDMA_SRC_INC_32 | UDMA_DST_INC_32 | UDMA_ARB_8);
	//trasferisci();
}
void transfer(){
	// Set up the transfer parameters for the software channel.  This will
	// configure the transfer buffers and the transfer size.  Auto mode must be
	// used for software transfers.
	uDMAChannelTransferSet(UDMA_CHANNEL_SW | UDMA_PRI_SELECT, UDMA_MODE_AUTO,
			g_ui32SrcBuf, g_ui32DstBuf,
			MEM_BUFFER_SIZE);
	// Now the software channel is primed to start a transfer.  The channel
	// must be enabled.  For software based transfers, a request must be
	// issued.  After this, the uDMA memory transfer begins.
	uDMAChannelEnable(UDMA_CHANNEL_SW);
	uDMAChannelRequest(UDMA_CHANNEL_SW);
}
int main(void) {
	FPULazyStackingEnable();
	ui32SysClkFreq = SysCtlClockFreqSet(
			(SYSCTL_XTAL_25MHZ | SYSCTL_OSC_MAIN | SYSCTL_USE_PLL
					| SYSCTL_CFG_VCO_480), 120000000);
	SysCtlPeripheralEnable(SYSCTL_PERIPH_UDMA);
	IntEnable(INT_UDMAERR);
	uDMAEnable();
	uDMAControlBaseSet(pui8ControlTable);
	InitSWTransfer();
	while (1) {
		transfer();
		SysCtlDelay(ui32SysClkFreq);
	}
}
So i applied the same "strategy " to udma_demo project
First of all i changed the project to work with SPI instead of UART and it works
Then i arranged it as i did for lab14 (partially disabled interrupt) but it seems it does not do anything; can you please help on that ?
Code is below:
/*
 * udma_spi.c
 *
 *  Created on: 05 nov 2016
 *      Author: Carlo
 *
 *
 *
 *
 *
 *
 *
 *
 */
//*****************************************************************************
//
// from udma_demo.c - uDMA example.
//
// Copyright (c) 2013-2016 Texas Instruments Incorporated.  All rights reserved.
// Software License Agreement
//
// Texas Instruments (TI) is supplying this software for use solely and
// exclusively on TI's microcontroller products. The software is owned by
// TI and/or its suppliers, and is protected under applicable copyright
// laws. You may not combine this software with "viral" open-source
// software in order to form a larger program.
//
// THIS SOFTWARE IS PROVIDED "AS IS" AND WITH ALL FAULTS.
// NO WARRANTIES, WHETHER EXPRESS, IMPLIED OR STATUTORY, INCLUDING, BUT
// NOT LIMITED TO, IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE APPLY TO THIS SOFTWARE. TI SHALL NOT, UNDER ANY
// CIRCUMSTANCES, BE LIABLE FOR SPECIAL, INCIDENTAL, OR CONSEQUENTIAL
// DAMAGES, FOR ANY REASON WHATSOEVER.
//
// This is part of revision 2.1.3.156 of the EK-TM4C1294XL Firmware Package.
//
//*****************************************************************************
#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_ints.h"
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "inc/hw_uart.h"
#include "inc/hw_ssi.h"
#include "driverlib/fpu.h"
#include "driverlib/gpio.h"
#include "driverlib/interrupt.h"
#include "driverlib/pin_map.h"
#include "driverlib/rom.h"
#include "driverlib/rom_map.h"
#include "driverlib/sysctl.h"
#include "driverlib/systick.h"
#include "driverlib/uart.h"
#include "driverlib/ssi.h"
#include "driverlib/udma.h"
#include "utils/cpu_usage.h"
#include "utils/uartstdio.h"
#include "utils/ustdlib.h"
//*****************************************************************************
//
//! \addtogroup example_list
//! <h1>uDMA (udma_demo)</h1>
//!
//! This example application demonstrates the use of the uDMA controller to
//! transfer data between memory buffers, and to transfer data to and from a
//! UART.  The test runs for 10 seconds before exiting.
//!
//! UART0, connected to the ICDI virtual COM port and running at 115,200,
//! 8-N-1, is used to display messages from this application.
//
//*****************************************************************************
#define CLOCH 1000000
//****************************************************************************
//
// System clock rate in Hz.
//
//****************************************************************************
uint32_t g_ui32SysClock;
//*****************************************************************************
//
// The number of SysTick ticks per second used for the SysTick interrupt.
//
//*****************************************************************************
#define SYSTICKS_PER_SECOND     100
//*****************************************************************************
//
// The size of the memory transfer source and destination buffers (in words).
//
//*****************************************************************************
#define MEM_BUFFER_SIZE         1024
//*****************************************************************************
//
// The size of the UART transmit and receive buffers.  They do not need to be
// the same size.
//
//*****************************************************************************
#define UART_TXBUF_SIZE         128
#define UART_RXBUF_SIZE         128
//*****************************************************************************
//
// The source and destination buffers used for memory transfers.
//
//*****************************************************************************
static uint32_t g_ui32SrcBuf[MEM_BUFFER_SIZE];
static uint32_t g_ui32DstBuf[MEM_BUFFER_SIZE];
//*****************************************************************************
//
// The transmit and receive buffers used for the UART transfers.  There is one
// transmit buffer and a pair of recieve ping-pong buffers.
//
//*****************************************************************************
static uint16_t g_ui8TxBuf[UART_TXBUF_SIZE];//CSB era uint8_t
static uint16_t g_ui8RxBufA[UART_RXBUF_SIZE];
static uint16_t g_ui8RxBufB[UART_RXBUF_SIZE];
//*****************************************************************************
//
// The count of uDMA errors.  This value is incremented by the uDMA error
// handler.
//
//*****************************************************************************
static uint32_t g_ui32uDMAErrCount = 0;
//*****************************************************************************
//
// The count of times the uDMA interrupt occurred but the uDMA transfer was not
// complete.  This should remain 0.
//
//*****************************************************************************
static uint32_t g_ui32BadISR = 0;
//*****************************************************************************
//
// The count of UART buffers filled, one for each ping-pong buffer.
//
//*****************************************************************************
static uint32_t g_ui32RxBufACount = 0;
static uint32_t g_ui32RxBufBCount = 0;
//*****************************************************************************
//
// The count of memory uDMA transfer blocks.  This value is incremented by the
// uDMA interrupt handler whenever a memory block transfer is completed.
//
//*****************************************************************************
static uint32_t g_ui32MemXferCount = 0;
//*****************************************************************************
//
// The CPU usage in percent, in 16.16 fixed point format.
//
//*****************************************************************************
static uint32_t g_ui32CPUUsage;
//*****************************************************************************
//
// The number of seconds elapsed since the start of the program.  This value is
// maintained by the SysTick interrupt handler.
//
//*****************************************************************************
static uint32_t g_ui32Seconds = 0;
//*****************************************************************************
//
// The control table used by the uDMA controller.  This table must be aligned
// to a 1024 byte boundary.
//
//*****************************************************************************
#if defined(ewarm)
#pragma data_alignment=1024
uint8_t pui8ControlTable[1024];
#elif defined(ccs)
#pragma DATA_ALIGN(pui8ControlTable, 1024)
uint8_t pui8ControlTable[1024];
#else
uint8_t pui8ControlTable[1024] __attribute__ ((aligned(1024)));
#endif
//*****************************************************************************
//
// The error routine that is called if the driver library encounters an error.
//
//*****************************************************************************
#ifdef DEBUG
void
__error__(char *pcFilename, uint32_t ui32Line)
{
}
#endif
//*****************************************************************************
//
// The interrupt handler for the SysTick timer.  This handler will increment a
// seconds counter whenever the appropriate number of ticks has occurred.  It
// will also call the CPU usage tick function to find the CPU usage percent.
//
//*****************************************************************************
void SysTickHandler(void) {
	static uint32_t ui32TickCount = 0;
	//
	// Increment the tick counter.
	//
	ui32TickCount++;
	//
	// If the number of ticks per second has occurred, then increment the
	// seconds counter.
	//
	if (!(ui32TickCount % SYSTICKS_PER_SECOND)) {
		g_ui32Seconds++;
	}
}
void uDMAErrorHandler(void) {
	uint32_t ui32Status;
	//
	// Check for uDMA error bit
	//
	ui32Status = ROM_uDMAErrorStatusGet();
	//
	// If there is a uDMA error, then clear the error and increment
	// the error counter.
	//
	if (ui32Status) {
		ROM_uDMAErrorStatusClear();
		g_ui32uDMAErrCount++;
	}
}
void uDMAIntHandler(void) {}
void SPI0IntHandler(void){
	uint32_t ui32Status;
	uint32_t ui32Mode;
	//
	// Read the interrupt status of the SPI.
	//
	ui32Status = ROM_SSIIntStatus(SSI0_BASE, 1);//eval board
	//
	// Clear any pending status, even though there should be none since no SPI
	// interrupts were enabled.  If SPI error interrupts were enabled, then
	// those interrupts could occur here and should be handled.  Since uDMA is
	// used for both the RX and TX, then neither of those interrupts should be
	// enabled. solo DMA-Int è enabled
	//
	ROM_SSIIntClear(SSI0_BASE, ui32Status);
	//
	//
	ui32Mode = ROM_uDMAChannelModeGet(UDMA_CHANNEL_SSI0RX | UDMA_PRI_SELECT);
	//
	//
	if (ui32Mode == UDMA_MODE_STOP) {
		//
		// Increment a counter to indicate data was received into buffer A.  In
		// a real application this would be used to signal the main thread that
		// data was received so the main thread can process the data.
		//
		g_ui32RxBufACount++;
		return;
		//
		// Set up the next transfer for the "A" buffer, using the primary
		// control structure.  When the ongoing receive into the "B" buffer is
		// done, the uDMA controller will switch back to this one.  This
		// example re-uses buffer A, but a more sophisticated application could
		// use a rotating set of buffers to increase the amount of time that
		// the main thread has to process the data in the buffer before it is
		// reused.
		//
		ROM_uDMAChannelTransferSet(UDMA_CHANNEL_SSI0RX | UDMA_PRI_SELECT,
		UDMA_MODE_BASIC, (void *) (SSI0_BASE + SSI_O_DR), g_ui8RxBufA,//CSB was UDMA_MODE_PINGPONG
		UART_RXBUF_SIZE);
		ROM_uDMAChannelEnable(UDMA_CHANNEL_SSI0RX);//added
	}
	//
	// If the SPI0 DMA TX channel is disabled, that means the TX DMA transfer
	// is done.
	//
	if (!ROM_uDMAChannelIsEnabled(UDMA_CHANNEL_SSI0TX)) {
		//
		// Start another DMA transfer to SPI0 TX.
		//
		g_ui8TxBuf[0]++;//added from tutorial
		ROM_uDMAChannelTransferSet(UDMA_CHANNEL_SSI0TX | UDMA_PRI_SELECT,
		UDMA_MODE_BASIC, g_ui8TxBuf, (void *) (SSI0_BASE + SSI_O_DR),
		UART_TXBUF_SIZE);//was sizeof(g_ui8TxBuf)
		//
		// The uDMA TX channel must be re-enabled.
		//
		ROM_uDMAChannelEnable(UDMA_CHANNEL_SSI0TX);
	}
}
void UART1IntHandler(void){};
void InitSPI0Transfer(void) {
	uint_fast16_t  ui16Idx;
	//
	// Fill the TX buffer with a simple data pattern.
	//
	for (ui16Idx = 0; ui16Idx < (UART_TXBUF_SIZE); ui16Idx++) {//in realtà è un array a 16 bit ora
		g_ui8TxBuf[ui16Idx] = 32000+ui16Idx;//e inizia a 32000
	}
	//
	// Enable the SPI peripheral
	//
	ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI0);
	//ROM_SysCtlPeripheralSleepEnable(SYSCTL_PERIPH_SSI0);
	//
	// Configure the SPI communication parameters.
	//
	GPIOPinConfigure(GPIO_PA2_SSI0CLK);
	GPIOPinConfigure(GPIO_PA3_SSI0FSS);
	GPIOPinConfigure(GPIO_PA4_SSI0XDAT0);
	GPIOPinConfigure(GPIO_PA5_SSI0XDAT1);
	GPIOPinTypeSSI(GPIO_PORTA_BASE, GPIO_PIN_5 | GPIO_PIN_4 | GPIO_PIN_3 |
			GPIO_PIN_2);
	ROM_SSIConfigSetExpClk(SSI0_BASE, g_ui32SysClock, SSI_FRF_MOTO_MODE_0,
			SSI_MODE_MASTER, CLOCH, 16);
	//
	// Enable the SPI for operation, and enable the uDMA interface for both TX
	// and RX channels.
	//
	ROM_SSIEnable(SSI0_BASE);
	while (SSIDataGetNonBlocking(SSI0_BASE, &g_ui32CPUUsage)) {
		}
	ROM_SSIDMAEnable(SSI0_BASE, SSI_DMA_TX | SSI_DMA_RX);
	//
	//HWREG(SSI0_BASE + SSI_O_CR1) |= SSI_CR1_LBM;// loopback
	//
	ROM_uDMAChannelAttributeDisable(UDMA_CHANNEL_SSI0RX,//CSB
	UDMA_ATTR_ALTSELECT | UDMA_ATTR_USEBURST |
	UDMA_ATTR_HIGH_PRIORITY |
	UDMA_ATTR_REQMASK);//check
	ROM_uDMAChannelControlSet(UDMA_CHANNEL_SSI0RX | UDMA_PRI_SELECT,
	UDMA_SIZE_16 | UDMA_SRC_INC_NONE | UDMA_DST_INC_16 |
	UDMA_ARB_4);
	ROM_uDMAChannelTransferSet(UDMA_CHANNEL_SSI0RX | UDMA_PRI_SELECT,
	UDMA_MODE_BASIC, (void *) (SSI0_BASE + SSI_O_DR), g_ui8RxBufA,//CSB change mode basic era UDMA_MODE_PINGPONG
	UART_RXBUF_SIZE);
	//
	// Put the attributes in a known state for the uDMA SPI0TX channel.  These
	// should already be disabled by default.
	//
	ROM_uDMAChannelAttributeDisable(UDMA_CHANNEL_SSI0TX,
	UDMA_ATTR_ALTSELECT |
	UDMA_ATTR_HIGH_PRIORITY |
	UDMA_ATTR_REQMASK);
	//
	ROM_uDMAChannelAttributeEnable(UDMA_CHANNEL_SSI0TX, UDMA_ATTR_USEBURST);
	//
	//
	ROM_uDMAChannelControlSet(UDMA_CHANNEL_SSI0TX | UDMA_PRI_SELECT,//CSB change size 16, inc 16;erano a 8
	UDMA_SIZE_16 | UDMA_SRC_INC_16 |
	UDMA_DST_INC_NONE |
	UDMA_ARB_4);//check
	//
	//
	ROM_uDMAChannelTransferSet(UDMA_CHANNEL_SSI0TX | UDMA_PRI_SELECT,
	UDMA_MODE_BASIC, g_ui8TxBuf, (void *) (SSI0_BASE + SSI_O_DR),
	UART_TXBUF_SIZE);
	//
	//
	ROM_uDMAChannelEnable(UDMA_CHANNEL_SSI0RX);
	ROM_uDMAChannelEnable(UDMA_CHANNEL_SSI0TX);
	//
	// Enable the SPI DMA TX/RX interrupts.
	//
	ROM_SSIIntEnable(SSI0_BASE, SSI_DMATX |SSI_DMARX);
	UARTprintf("start Init\n");
	//
	// Enable the SPI peripheral interrupts.
	//
	ROM_IntEnable(INT_SSI0);
	UARTprintf("end Init\n");
}
//*****************************************************************************
//
// Initializes the uDMA software channel to perform a memory to memory uDMA
// transfer.
//
//*****************************************************************************
void InitSWTransfer(void) {}
//*****************************************************************************
//
// Configure the UART and its pins.  This must be called before UARTprintf().
//
//*****************************************************************************
void ConfigureUART(void) {
	//
	// Enable the GPIO Peripheral used by the UART.
	//
	ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
	//
	// Enable UART0
	//
	ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
	ROM_SysCtlPeripheralSleepEnable(SYSCTL_PERIPH_UART0);
	//
	// Configure GPIO Pins for UART mode.
	//
	ROM_GPIOPinConfigure(GPIO_PA0_U0RX);
	ROM_GPIOPinConfigure(GPIO_PA1_U0TX);
	ROM_GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
	//
	// Initialize the UART for console I/O.
	//
	UARTStdioConfig(0, 115200, g_ui32SysClock);
}
void data_transfer(){
	ROM_uDMAChannelTransferSet(UDMA_CHANNEL_SSI0RX | UDMA_PRI_SELECT,
	UDMA_MODE_BASIC, (void *) (SSI0_BASE + SSI_O_DR), g_ui8RxBufA,
	UART_RXBUF_SIZE);
	ROM_uDMAChannelTransferSet(UDMA_CHANNEL_SSI0TX | UDMA_PRI_SELECT,
	UDMA_MODE_BASIC, g_ui8TxBuf, (void *) (SSI0_BASE + SSI_O_DR),
	UART_TXBUF_SIZE);
	ROM_uDMAChannelEnable(UDMA_CHANNEL_SSI0RX);
	ROM_uDMAChannelEnable(UDMA_CHANNEL_SSI0TX);
}
int main(void) {
	static uint32_t ui32PrevSeconds;
	static uint32_t ui32PrevXferCount;
	static uint32_t ui32PrevUARTCount = 0;
	uint32_t ui32XfersCompleted;
	uint32_t ui32BytesTransferred;
	//
	// Set the clocking to run directly from the crystal at 120MHz.
	//
	g_ui32SysClock = MAP_SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ |
	SYSCTL_OSC_MAIN |
	SYSCTL_USE_PLL |
	SYSCTL_CFG_VCO_480), 120000000);
	//
	// Enable peripherals to operate when CPU is in sleep.
	//
	//ROM_SysCtlPeripheralClockGating(true);
	//
	// Enable the GPIO port that is used for the on-board LED.
	//
	ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPION);
	//
	// Enable the GPIO pins for the LED (PN0).
	//
	ROM_GPIOPinTypeGPIOOutput(GPIO_PORTN_BASE, GPIO_PIN_0);
	//
	// Initialize the UART.
	//
	ConfigureUART();
	UARTprintf("\033[2J\033[H");
	UARTprintf("uDMA Example\n");
	//
	// Show the clock frequency on the display.
	//
	UARTprintf("Tiva C Series @ %u MHz\n\n", g_ui32SysClock / 1000000);
	//
	// Configure SysTick to occur 100 times per second, to use as a time
	// reference.  Enable SysTick to generate interrupts.
	//
	ROM_SysTickPeriodSet(g_ui32SysClock / SYSTICKS_PER_SECOND);
	ROM_SysTickIntEnable();
	ROM_SysTickEnable();
	//
	// Initialize the CPU usage measurement routine.
	//
	//CPUUsageInit(g_ui32SysClock, SYSTICKS_PER_SECOND, 2);
	//
	// Enable the uDMA controller at the system level.  Enable it to continue
	// to run while the processor is in sleep.
	//
	ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UDMA);
	//ROM_SysCtlPeripheralSleepEnable(SYSCTL_PERIPH_UDMA);
	//
	// Enable the uDMA controller error interrupt.  This interrupt will occur
	// if there is a bus error during a transfer.
	//
	ROM_IntEnable(INT_UDMAERR);
	//
	// Enable the uDMA controller.
	//
	ROM_uDMAEnable();
	//
	// Point at the control table to use for channel control structures.
	//
	ROM_uDMAControlBaseSet(pui8ControlTable);
	//
	// Initialize the uDMA UART transfers.
	UARTprintf("SPI0transfer\n");
	//
	InitSPI0Transfer();
	//
	// Indicate on the display that the example is stopped.
	//
	UARTprintf("\nStopped\n");
	//
	// Disable uDMA and UART interrupts now that the test is complete.
	//
	//ROM_IntDisable(INT_SSI0);//multitasking
	//ROM_IntDisable(INT_UDMA);
	//
	// Loop forever with the CPU not sleeping, so the debugger can connect.
	//
	while (1) {
		//
		// Turn on the LED.
		//
		GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_0, GPIO_PIN_0);
		//
		// Delay for a bit.
		//
		SysCtlDelay(g_ui32SysClock  );
		//
		// Turn off the LED.
		//
		GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_0, 0);
		//
		// Delay for a bit.
		//
		SysCtlDelay(g_ui32SysClock );
		data_transfer();//my function
		UARTprintf(" tx %i \n",g_ui8TxBuf[0]);
		UARTprintf(" rx %i \n",g_ui8RxBufA[0]);
	}
}