Other Parts Discussed in Thread: TMS570LS1114
I'm attempting to interface my TMS570LS1114 to a DS1621 via I2C. I have included my send and recieve routines below based on the HAL CoGen drivers. Currently the send routine appears to be working, but I am having trouble with receive since it requires a repeated start. I appreciate any input.
void DS1621::I2CSend(uint8 Cmd, uint32 length, uint8 * data)
{
//config
/* Set mode as Master */
i2cSetMode(i2cREG1, I2C_MASTER);
i2cSetDirection(mNode, I2C_TRANSMITTER);
i2cSetSlaveAdd(mNode, SlaveAddr);
i2cSetCount(mNode, length+1);
i2cSetStop(mNode);
//send
i2cSetStart(mNode);
i2cSendByte(mNode, Cmd);
i2cSend(mNode, length, data);
/* Wait until Bus Busy is cleared */
while(i2cIsBusBusy(mNode) == true);
/* Wait until Stop is detected */
while(i2cIsStopDetected(mNode) == 0);
/* Clear the Stop condition */
i2cClearSCD(mNode);
}
void DS1621::I2CRcv(uint8 Cmd, uint32 length, uint8 * data)
{
//config
i2cSetMode(i2cREG1, I2C_MASTER);
i2cSetDirection(mNode, I2C_TRANSMITTER);
i2cSetSlaveAdd(mNode, SlaveAddr);
i2cSetCount(mNode, length+1);
i2cSetStop(mNode);
//send
i2cSetStart(mNode);
i2cSendByte(mNode, Cmd);
/* Wait until Bus Busy is cleared */
// while(i2cIsBusBusy(mNode) == true);
//reconfig
i2cSetDirection(mNode, I2C_RECEIVER);
//receive
i2cSetStart(mNode);
i2cReceive(mNode, length, data);
/* Wait until Bus Busy is cleared */
while(i2cIsBusBusy(mNode) == true);
/* Wait until Stop is detected */
while(i2cIsStopDetected(mNode) == 0);
/* Clear the Stop condition */
i2cClearSCD(mNode);
}