Other Parts Discussed in Thread: MIKROELEKTRONIKA
Hello
I generated a hex file after compiling my code in CCS-6 in release mode. I have ARM XDS100v2 as a debugger, also I have Mikroelektronika programmer. When i used Mikroelektronika programmer to program micro controller, it got programmed but it is not functioning. when I used ARM XDS100v2 debugger to load the same code works fine.
Another thing is, by using Mikroelektronika programmer if I read hex file from controller (which is already loaded using ARM XDS100v2 ) and save it. That saved hex file i am able to program using Mikroelektronika programmer, this time it is functioning fine.
So what is the difference between these two hex files : one is generated after building code in CCS-6 and other one is loaded by ARM XDS100v2 and read from controller using Mikroelektronika programmer.
Why Mikroelektronika programmer cannot program the controller the hex file generated by CCS-6 compilation