Hi Guys,
I'd like to shut down a high voltage / high current IGBT inverter output in highly dependable way.
The IGBT driver controlled by a 3 phase ePWM peripherial and it has an ENABLE/RESET input, but I don't want to rely on just one mechanism so I 'd like to switch off the PWM generation next to using IGBT ENABLE signal. The safe state is low or highz.
Options:
- Continuous Software Force on PWM output A and B low.
- Stop PWM by software Tripzone and force output to low or highz.
- Configure PWM multiplexer to GPIO input (highz).
- Configure PWM multiplexer to GPIO output low.
What is your opinion, which option (or combination of options) is the most reliable way for disabling PWM output?
Thank you, regards: Szilárd