This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAP error (Error -1170 @ 0x0)

Hi there,

I am trying to debug a second design based on 1294. I am using the latest CCS and Windows 10, and I use both Olimax and Spectrum Digital's XDS100V3

I tried it on two home made boards, which are running on 250ppm 25Mhz clock source instead of the normal 50ppm crystal (could this be the problem? I may have missed it but I did't find any spec on this issue)

After the program is flashed in, it has about 50/50 chance to start properly.

when it fails,  CCS shows the following error:

Error connecting to the target:
(Error -1170 @ 0x0)
Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK).

Where should I look into to track down this problem?

Thanks!