This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC DMA

Dear All

I am trying to get data from an RGB sensor and transfer the same to UART for Processing in the GUI, I am triggering the ADC by PWM which is about 500Khz 

My Plan is  to do a DMA transfer from the ADC0 FIFO to a Array and then to the Serial Port 

how ever i am unable to get the data from the FIFO to the ARRAY here is the code for the same pls correct me if i have gone wrong some where

///////////////ADC Configuration for A0,A1,A2/////////////////////
ADCClockConfigSet(ADC0_BASE, ADC_CLOCK_SRC_PIOSC | ADC_CLOCK_RATE_FULL, 1);
ADCSequenceConfigure(ADC0_BASE,1,ADC_TRIGGER_PWM_MOD0|ADC_TRIGGER_PWM1, 0);
ADCSequenceStepConfigure(ADC0_BASE, 1, 0, ADC_CTL_CH0);
ADCSequenceStepConfigure(ADC0_BASE, 1, 1, ADC_CTL_CH1);
ADCSequenceStepConfigure(ADC0_BASE, 1, 2, ADC_CTL_CH2 | ADC_CTL_IE | ADC_CTL_END);
ADCSequenceEnable(ADC0_BASE, 1);
ADCIntClear(ADC0_BASE, 1);
ADCIntEnable(ADC0_BASE, 1);


//////////////////////////uDMA Enable for ADC Values

uDMAEnable();
uDMAControlBaseSet(udmaCtrlTable);
ADCSequenceDMAEnable(ADC0_BASE,1);
uDMAChannelAttributeDisable(UDMA_CHANNEL_ADC0, UDMA_ATTR_ALTSELECT | UDMA_ATTR_HIGH_PRIORITY | UDMA_ATTR_REQMASK);
uDMAChannelAttributeEnable(UDMA_CHANNEL_ADC0, UDMA_ATTR_USEBURST);
uDMAChannelControlSet(UDMA_CHANNEL_ADC0 | UDMA_PRI_SELECT, UDMA_SIZE_32 | UDMA_SRC_INC_NONE | UDMA_DST_INC_32 | UDMA_ARB_1024);
uDMAChannelControlSet(UDMA_CHANNEL_ADC0 | UDMA_ALT_SELECT, UDMA_SIZE_32 | UDMA_SRC_INC_NONE | UDMA_DST_INC_32 | UDMA_ARB_1024);
uDMAChannelTransferSet(UDMA_CHANNEL_ADC0 | UDMA_PRI_SELECT, UDMA_MODE_PINGPONG, (void *)(ADC0_BASE + ADC_O_SSFIFO0), &Receive_Buff, ADC_SAMPLE_BUF_SIZE);
uDMAChannelTransferSet(UDMA_CHANNEL_ADC0 | UDMA_ALT_SELECT, UDMA_MODE_PINGPONG, (void *)(ADC0_BASE + ADC_O_SSFIFO0), &Receive_Buff, ADC_SAMPLE_BUF_SIZE);
uDMAChannelEnable(UDMA_CHANNEL_ADC0);
ADCIntEnable(ADC0_BASE, 1);