Other Parts Discussed in Thread: UNIFLASH, TMS570LS0914, TMS570LS1114
In short files
ccsv6\ccs_base\hercules\flash\configs\TMS570LS0x14.xml
and
uniflash_3.4\ccs_base\hercules\flash\configs\TMS570LS0x14.xml
has invlalid flash map for TMS570LS0914.
This map contains only 11 sectors, but TMS570LS0914 has 13 sectors in BANK 0
This lead to errors when I try to fill all flash memory with valid ECC
CortexR4: Erasing Flash Bank 0, Sector 11
CortexR4: Verifying Flash @ Address 0x0009FF00 of length 0x00007FF0
CortexR4: Writing Flash @ Address 0x000a7ef0 of Length 0x00007ff0
CortexR4: Verifying Flash @ Address 0x000A7EF0 of length 0x00007FF0
CortexR4: Writing Flash @ Address 0x000afee0 of Length 0x00007ff0
CortexR4: Verifying Flash @ Address 0x000AFEE0 of length 0x00007FF0
CortexR4: Writing Flash @ Address 0x000b7ed0 of Length 0x00007ff0
CortexR4: Verifying Flash @ Address 0x000B7ED0 of length 0x00007FF0
CortexR4: Writing Flash @ Address 0x000bfec0 of Length 0x00007ff0
CortexR4: File Loader: Memory write failed: The address 0xc7eaf does not map to a valid Flash Bank
CortexR4: GEL: File: C:\auto\platform_tx\tx_io_body_control\Debug\tx_io_body_control.out: Load failed.
CortexR4: GEL Output: Memory Map Setup for Flash @ Address 0x0 due to System Reset