This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Flexray Example Node A node B

Hi,

I am running the Flexray Example Code for Two nodes on two TMS570LS12, it seems to be working "fine" but I am wondering if there is any explanation of the Example code so I know what information that is expected to see, and what the code is supposed to do.

Im trying to analyse the communication with a Picoscope but I am struggling to decode the serial communication. I also cant see in the code what Baudrate this is configured to communicate over, trying to decode at 10Mbps. Do anyone know what Baudrate this is set to communicate over.

I have about 95 Ohm between the BP and BM lines. (Left out R11, R10, R19 and R20 on the FR/CAN/LIN daughter card on one of the nodes)

You can see a picuture of what I managed to capture from the waveform here: