This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BMP085 Reading for TM4C123 based controller

Could not get pressure or temperature measurements using BMP085, any problem in the code. Thanks



// BMP085 -- Atmospheric Pressure / Altitude Sensor

#include "defines.h"

#define BMP085_ADDRESS        0x77
#define START                0x00000007
#define REPEATED_START        0x0000000b
#define CONT                0x00000009
#define STOP                0x00000005
#define MEASURE_TEMP        0x2e
#define MEASURE_PRESSURE    0x34
#define BMP_START_MEASURE    0xf4
#define BMP_READ_MEASURE    0xf6

const unsigned char OSS = 0;

typedef struct
{
    short    ac1,ac2,ac3,b1,b2,mb,mc,md;
    unsigned short ac4,ac5,ac6;
}coeffs;

typedef struct
{
    long temp, pressure;
} BMP_vals;


const unsigned char OSS = 0;
long b5;
//short *ut;


// start measurement seq for ut and up
void start_measurement(unsigned char device_addr, unsigned char EEPROM_addr, unsigned char cmd)
{
    I2C1_MSA_R=device_addr;
    I2C1_MCS_R=START;
    I2C1_MDR_R=EEPROM_addr;
    while (I2C1_MCS_R & I2C_MCS_BUSY);
    I2C1_MDR_R=cmd;
    I2C1_MCS_R=STOP;
    while (I2C1_MCS_R & I2C_MCS_BUSY);
}


// get values of ut and up from the device
unsigned char *get_measurement(unsigned device_addr, unsigned EEPROM_addr,int no_bytes)
{
    static unsigned char ch[3];
    I2C1_MSA_R=device_addr;
    I2C1_MCS_R=START;
    I2C1_MDR_R=EEPROM_addr;
    while (I2C1_MCS_R & I2C_MCS_BUSY);
    I2C1_MCS_R=STOP;
    while (I2C1_MCS_R & I2C_MCS_BUSY);
    I2C1_MSA_R=device_addr+1;
    I2C1_MCS_R=REPEATED_START;
    while (I2C1_MCS_R & I2C_MCS_BUSY);
    ch[0]=I2C1_MDR_R;
    if (no_bytes==3)
    {
        I2C1_MCS_R=CONT;
        while (I2C1_MCS_R & I2C_MCS_BUSY);
        ch[1]=I2C1_MDR_R;
        I2C1_MCS_R=STOP;
        while (I2C1_MCS_R & I2C_MCS_BUSY);
        ch[2]=I2C1_MDR_R;
    }
    else
    {
    I2C1_MCS_R=STOP;
    while (I2C1_MCS_R & I2C_MCS_BUSY);
    ch[1]=I2C1_MDR_R;
    }
    return ch;
}


//read no of bytes from the device
unsigned char *get_chars(unsigned char slave_addr, unsigned char start_addr, int len)
{
    static unsigned char ch_ptr[50];
    int i;

    I2C1_MSA_R=slave_addr<<1;
    I2C1_MCS_R=START;
    I2C1_MDR_R=start_addr;
    while (I2C1_MCS_R & I2C_MCS_BUSY);
    I2C1_MSA_R=slave_addr<<1+1;
    I2C1_MCS_R=REPEATED_START;
    while (I2C1_MCS_R & I2C_MCS_BUSY);
    ch_ptr[0]=I2C1_MDR_R;
    for (i=1;i<len-1;i++)
    {
        I2C1_MCS_R=CONT;
        while (I2C1_MCS_R & I2C_MCS_BUSY);
        ch_ptr[i]=I2C1_MDR_R;
    }
    I2C1_MCS_R=STOP;
    while (I2C1_MCS_R & I2C_MCS_BUSY);
    ch_ptr[len-1]=I2C1_MDR_R;
    return ch_ptr;
}




//calc temperature
int calc_temp(short ut, coeffs *BMP_coeffs)
{
      long x1, x2;
//      coeffs *BMP_coeffs;
      x1 = (((long)ut - (long)BMP_coeffs->ac6)*(long)BMP_coeffs->ac5) >> 15;
      x2 = ((long)BMP_coeffs->mc << 11)/(x1 + BMP_coeffs->md);
      b5 = x1 + x2;
      return ((b5 + 8)>>4);
}

//calc presssure
long calc_pressure(long up, coeffs *BMP_coeffs)
{
      long x1, x2, x3, b3, b6, p;
      unsigned long b4, b7;

      b6 = b5 - 4000;
      // Calculate B3
      x1 = (BMP_coeffs->b2 * (b6 * b6)>>12)>>11;
      x2 = (BMP_coeffs->ac2 * b6)>>11;
      x3 = x1 + x2;
      b3 = (((((long)BMP_coeffs->ac1)*4 + x3)<<OSS) + 2)>>2;

      // Calculate B4
      x1 = (BMP_coeffs->ac3 * b6)>>13;
      x2 = (BMP_coeffs->b1 * ((b6 * b6)>>12))>>16;
      x3 = ((x1 + x2) + 2)>>2;
      b4 = (BMP_coeffs->ac4 * (unsigned long)(x3 + 32768))>>15;

      b7 = ((unsigned long)(up - b3) * (50000>>OSS));
      if (b7 < 0x80000000)
        p = (b7<<1)/b4;
      else
        p = (b7/b4)<<1;

      x1 = (p>>8) * (p>>8);
      x1 = (x1 * 3038)>>16;
      x2 = (-7357 * p)>>16;
      p += (x1 + x2 + 3791)>>4;

      return p;
}



BMP_vals get_BMP_vals (void)
{
//    int    temp;
    short *ut;
    long temp,pressure,*up;
    coeffs *BMP_coeffs;
    BMP_vals val;
    BMP_coeffs=(coeffs*)get_chars(BMP085_ADDRESS,0xaa,22);
    start_measurement(BMP085_ADDRESS,BMP_START_MEASURE,MEASURE_TEMP);
    delay(_5ms);
    ut=(short*)get_measurement(BMP085_ADDRESS,BMP_READ_MEASURE,2);
    start_measurement(BMP085_ADDRESS,BMP_START_MEASURE,MEASURE_PRESSURE);
    delay(_5ms);
    up=(long*)get_measurement(BMP085_ADDRESS,BMP_READ_MEASURE,3);
    val.temp=calc_temp(*ut,BMP_coeffs);
    val.pressure=calc_pressure(*up,BMP_coeffs);
    return val;
}