Other Parts Discussed in Thread: TM4C1294KCPDT
Customer has two other devices connected to the TM4C1294KCPDT that when they are initialized pins PE1 and PE2 configured as inputs are driven to 1.8V level for about 500 ms.. Customer wants to confirm that this will not damage the device. Customer understand that during this time the logic state is invalid and is ignored. Pin configuration is as follows:
GPIOTiva_PE_2 | GPIO_CFG_INPUT | GPIO_CFG_IN_NOPULL,
GPIOTiva_PE_1 | GPIO_CFG_INPUT | GPIO_CFG_IN_NOPULL,