Other Parts Discussed in Thread: LM3S6432
Hi All. I met very strange thing with TIVA controller. Our company develop and produce IoT devices. We used lm3s6432 controller earlier. But now we are replacing on TM4C1294KCPTDT. Half a year ago we produced 65 devices for testing (one project). And now 7 devices were broken. They have same sign - almost all vdd pins short circut to gnd. The power circuit the same when we used Luminary. Main power is 12V then mc3363 convert to 5.0V, then 1117-33 to 3.3V. After replacing only MCU a device is working very well. We produced 3000 devices based on Luminary, and not had such troubles.
short circuit to gnd have next pins:
- 7, 16, 26, 28, 39, 47, 51, 69, 79, 90, 101, 113, 122 (they all VDD pins)
- GND and GNDA (normal)
don't have:
- 52 (VDD!!!), 87(VDDC), 115(VDDC), 8(VDDA), 9(VREFA+), 68(VBAT) and other pins.
Please help me to resolve my problem as soon as possible. Ready to shipment new 35 devices based on TIVA to end customer. Our company produce 25 different devices based on ethernet (Luminary). Our engineers replaced LM3S controllers in our projects and are testing new PCBs. We have only 150 pcs new controllers LM3S6432 for produced. At next year we have to produce all devices only based on Tiva controllers. We have alredy bought 540 pcs TM4C1294 controllers at local distributor.
Alex Pas
avp-electro.com